cancel
Showing results for 
Search instead for 
Did you mean: 

Problem reading value gyroscope

Patrick Giacomino
Associate
Posted on January 27, 2017 at 15:04

Hello, sorry for me level in English

I have to carry out an end of year project of electronic bts, and I am stuck at this level

I need your help to understand a lack of reading in the following code

 I use this soft : 'Sensors_Reader', it is a program provided on the page of the site MBED

I have this board NUCLEO_L476RG and this shield sensors 'X-NUCLEO-IKS01A1'

I receive this information in return on 'un moniteur serie' :

--- Starting new run ---

Humidity | Temperature Sensor ID = HTS221 (0xbc | 0xbc)

Gyroscope | Motion Sensor ID = UNKNOWN (0x0 | 0x0)

===

I2C [errors]: 0x00       X                Y                Z

MAG [mgauss]:          0          536872992      214

ACC [mg]:                   0                0          134247283

GYR [mdps]:                 0                0                   5

---

TEMP | HUMIDITY:    27.54°C | 25.72%

TEMP | PRESSURE: 0.00°F | 0.00mbar

===

The problem is that I do not have the pressure values, can you help me to fix this problem

I have attached the contents of the program

#x-nucleo-iks01a2 #lps22hb
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0