Posted on January 31, 2017 at 06:12hi, I am Reading the Accelerometer and Gyroscope sensor values by checking the XLDA and GDA bits as follows if((readReg(STATUS_REG)&0x01)==0x01) // checking XLDA { Ax = (int1...
Posted on January 23, 2017 at 13:03Hi, I am using STEVAL-MKI160V1 evaluation module of LSM6DS3 in arduino platform with 8g scale. When I turn this 1g to -1g , it suddenly fall to 89 , 86 , 89.......etc , from 4173 (1g reading, that i got) w...
Posted on December 23, 2016 at 07:27Hi, I am new to LSM6DS3 inertial module, I am trying to use it with my arduino mega 2560, in SPI mode ,but in trouble with Z & Y axis output of the accelero meter. X axis output respond well.Already tried to read...
Posted on December 23, 2016 at 15:43Changed the value in CTRL3_C to 0x41 , attaching the images of output values of x,y,z of accelero , all axis are tested with +1g, x gives perfect output, z and y gives some valid output when i give some knock on...