MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

6D orientation detection with LIS3DH

Posted on February 03, 2017 at 16:40Hi all,I'm using a LIS3DH accelerometer and I would like to detect the device orientation in the space. According to the specifications I could do this by means of the 6D orientation detection function, but I'm no...

Precision difference between LPS22HB and LPS25HB

Posted on October 29, 2016 at 12:25Hi, I can read from LPS25HB ST description page that it have ''High-resolution mode: 0.01 hPa RMS'' while on LPS22HB there's nothing about this. But looking at either datasheed I've found that: LPS22HB PAccT +/-0.1...

VL53L0X measurement profile/spec

Posted on June 30, 2017 at 22:32Hi,changing the timing budget affects the measurment accurancy/speed/range.  This is done with the function VL53L0_SetMeasurementTimingBudgetMicroSeconds(..). Does this function affects the measurements parameter in t...

dialogue by Associate
  • 1582 Views
  • 2 replies
  • 0 kudos

LIS2HH12 Noise Information

Posted on August 16, 2016 at 17:37Hi, I've a design based on LIS344ALH where the noise level is a very sensitive parameter since I need to measure signals in the mg range. I would like to move to a full digital component and I'm looking to the LIS2H...

cn2 by Associate II
  • 3129 Views
  • 7 replies
  • 0 kudos

LIS3DH accelerometer sensitivity in low power mode

Posted on July 17, 2015 at 15:05Hello,I am planning to operate the LIS3DH accelerometer in low power mode (resulting in an output data rate of 5kHz according to Table 26 in the datasheet).In Table 3 in the datasheet a sensitivity of 12mg/digit is gi...

stephan by Associate
  • 2379 Views
  • 3 replies
  • 0 kudos

LIS3DH 5kHz ODR not possible

Posted on May 09, 2016 at 15:33Hello all, I want to use the LIS3DH accelerometer and a Steval-MK1109v2 Motherboard with the ST Unico GUI for logging Acceleration data. The datasheet of the LIS3DH shows the possibility to meassure a bandwidth up to ...

www.st.com

Posted on August 11, 2017 at 19:00Hello,  I am trying to use the http://www.st.com/en/evaluation-tools/steval-mki129v1.html board on a breadboard.  It has a http://www.st.com/en/audio-ics/mp45dt02-m.html.  I am trying to resolve the two data sheets ...

0690X00000603hJQAQ.jpg 0690X000006040JQAQ.jpg 0690X000006040TQAQ.jpg

Resolved! MEMS pdm microphone - custom board

Posted on August 10, 2017 at 13:33Hi community!So far i have been developing my audio application on discovery board STM32F407 (there is a embedded MEMS microphone connected to I2S2), I have been able to configure I2S2 periphery and acquire data wit...

aci_gatt_update_char_value Failing For IDB05A1

Posted on August 06, 2017 at 20:02I have an IDB05A1 using aci_gatt_update_char_value. This call works for anything using 4 byte array sizes or smaller, but it returns BLE_STATUS_ERROR for arrays larger than this. I'm calling both aci_gatt_init and a...

hushel by Associate II
  • 780 Views
  • 0 replies
  • 0 kudos

State Machine programming for LSM330

Posted on February 15, 2017 at 06:13I am looking for some code examples or technical notes on programming the state machine in LSM330TR but couldn't find any in ST.com. Has anyone found these ? Could you please share if you have.#lsm330-state-machin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.