MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH Z output noisy

Posted on June 05, 2017 at 11:40I am trying to measure a machine's vibration using LIS3DH sensor. I set the LIS3DH in low power mode and 5.376 kHz sampling frequency which outputs 8 bit output. I use spi to get the data from the sensor. I changed th...

0690X00000607ETQAY.png

LSM6DS0 failing to generate interrupt

Posted on July 02, 2017 at 14:49Hi everyone, we are working the the LSM6DS0 from ST interfacing through SPI with a CC2650 microcontroller. We have been able to test our custom PCB, read some data from the accelerometer, but we are not able to config...

VL53L0X sensor timeout in API

Posted on June 30, 2017 at 19:28Hey guys I have been working with VL53L0X and Stm32F7  at my company so the problem is that it can identify the chip ID well but get a ERROR_CONTROL_INTERFACE at the first api callVL53L0X_DataInit(&MyDevice);After fur...

psalian by Associate II
  • 1105 Views
  • 0 replies
  • 0 kudos

Resolved! Hi, I have bought X-NUCLEO-IKS01A1 having 4 sensors,I have see that X-NUCLEO-IKS01A1 is arduino uno compatible,How to interface that board with arduino UNO , I have tried the interfacing same like ST nucleio board but couldn't find the address detecting,P

Posted on June 22, 2017 at 18:21Hi,I have X-NUCLEO-IKS01A1 having 4 MEM sensors ,I have seen that this board is compatible with arduino UNO,I have connected the board same as like the ST nucleio board,but I couldn't find the sensors giving output wi...

LSM9DS1 FIFO behavior

Posted on June 28, 2017 at 12:38Hi, I'm having some problem using the LSM9DS1 FIFO...My objective is to continuously acquire, without loosing samples, the Gyro and Accelleration data. (The magnetometer is turned off)This is what I do:- I set the wat...

STM32F072 usb audio

Posted on May 19, 2016 at 04:45 Hi guys, I new to STM32, was mostly use PIC32 for USB audio application but due to cost decided to switch to STM Now I have STM32F0 discovery board with STM32F072RBT6. I tried to setup USB audio w...

sgpiqx by Associate II
  • 4767 Views
  • 9 replies
  • 0 kudos

LSM6DS3 : Who-Am-I value not valid

Posted on June 23, 2017 at 15:24Hello,I am interfacing SPI based LSM6DS3 accelerometer to imx7 based board. I got LSM6DS3 driver from  'https://github.com/STMicroelectronics/STMems_Linux_Input_drivers '. Added device tree for this (kernel-4.1.15) as...

LIS331HH, understanding self test

Posted on June 22, 2017 at 14:51We have two prototype boards each equipped with a LIS331HH.One of the sensors seems completely broken because the Z axis shows values around 2.3g while laying flat on the table. Because of that we were now looking int...

Daniel S. by Associate III
  • 1899 Views
  • 1 replies
  • 0 kudos

Request of VL53L0X

Posted on December 29, 2016 at 08:41Hello,I am using VL53L0X to perform range measurement. I knew there are C APIs and examples that provided by ST already. However, due to I am developing my project by other language, I think I should access to reg...

HTS221 driver integration for imx6

Posted on June 21, 2017 at 12:34Hi,I'm having trouble with HTS221 device driver integration (for a FreeRTOS app). ST provides a platform independent driver (see http://www.st.com/en/mems-and-sensors/hts221.html ). But those drivers have functions wh...