2016-08-04 2:54 AM
Hi,
I'm working on lsm9ds0 and spi with a stm32f4. The accelerometer and gyroscope work successfully on my device but since a few days, the magnetometer seems to get random values. For test, gyroscope is in power down mode. This is my configuration : lsm9_driver_write_register(LSM9DS0_CTRL_REG1_XM, (0x60)|(0x07)); // ODR 100HZ, enable all axis, continuous update lsm9_driver_write_register(LSM9DS0_CTRL_REG2_XM, 0b00100000 ); // ±16 g lsm9_driver_write_register(LSM9DS0_CTRL_REG5_XM, (0x80)|(0x14) );// temp enable, low resoluation mag, 100Hz ODR lsm9_driver_write_register(LSM9DS0_CTRL_REG6_XM, 0b00000000, ); // ±2gauss lsm9_driver_write_register(LSM9DS0_CTRL_REG7_XM, 0b10000000); // normal mode lsm9_driver_write_register(LSM9DS0_OFFSET_X_L_M, 0x00); lsm9_driver_write_register(LSM9DS0_OFFSET_X_H_M, 0x00); lsm9_driver_write_register(LSM9DS0_OFFSET_Y_L_M, 0x00); lsm9_driver_write_register(LSM9DS0_OFFSET_Y_H_M, 0x00); lsm9_driver_write_register(LSM9DS0_OFFSET_Z_L_M, 0x00); lsm9_driver_write_register(LSM9DS0_OFFSET_Z_H_M, 0x00); lsm9_driver_write_register(LSM9DS0_REFERENCE_X, 0x00); lsm9_driver_write_register(LSM9DS0_REFERENCE_Y, 0x00); lsm9_driver_write_register(LSM9DS0_REFERENCE_Z, 0x00); Read configuration and transmitted by uart : http://img110.xooimage.com/files/0/a/f/configlsm9-5011236.pngExtract of data send by uart : http://img110.xooimage.com/files/7/5/7/data-5011237.pngWhen i move sensor, accelerometer values correctly change but the values on magnetometer stay random. In doubt, i use a magnet in proximity, nothing changes. Moreover, four sensors have the same phenomenon of random values.