2016-08-07 4:03 AM
Hello,
1.according to section 2.11 Temperature sensor :should i read both OUT_TEMP_L (0Ch) & OUT_TEMP_H (0Dh) ?the data is stored only in OUT_TEMP_H (0Dh) ?2.the data i get using OUT_TEMP_H (0Dh) is too low (10C-13C), where the room temperature should be about 20C, am i reading the data wrong?RegardsAmir2016-08-08 1:36 AM
The temperature sensor can be used to measure temperature variations. It isn't suitable to return absolute temperatures measures.
The value represents difference respect to a reference not specified value.
Do following to correctly work with temperature sensor:
- enable the bits 6 and 7 in TEMP_CFG_REG(1Fh): enable aux ADC and enable temperature sensor.
- enable Block Data Update, BDU, feature. CTRL_REG4(0x23) , BDU (bit#7)=1.
- read both the ADC output 3 registers (because of BDU enabled): OUT_ADC_3_L(0x0C) and OUT_ADC_3_H(0x0D).
Data representation: 2's complement.
Useful bits: 8, left aligned, hence useful data in OUT_ADC_3_H.
Temperature sensor output change vs temperature: 1digit/degrCelsius
Best regards
Miroslav