LIS2DW12 accelerometer Arduino
Hi I am looking for example code for the LIS2DW12 using Arduino code . I am using an Expressiff module esp32 C3 Does anyone have some example code ?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi I am looking for example code for the LIS2DW12 using Arduino code . I am using an Expressiff module esp32 C3 Does anyone have some example code ?
We want to use the Sensor TileBox pro to measure temp pressure and acceleration in structures. We have been using some of your boards the MKI versions and they will run at a maximum of 1400 time steps per second when configured for about 2000. I ...
Hello. I have LIS2DUX12 accelerometer and have sucessfully ran machine learning example from STMems (activity_recognition_for_mobile) on our custom hardware.https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lis2dux12_STdC/ex...
Hello,We have the ISM330DHCX designed into a new product but I am having trouble getting reliable readings using the I2C interface. I am able to read the WHOAMI register and get 0x6B but OUT_TEMP_L (20h), OUT_TEMP_H (21h) always return zero.I have th...
Hi everyone,I am working with the LSM6DSM and an external LIS3MDL magnetometer and have the FIFO ODR set to 208 Hz, with no decimation configured.I am trying to understand exactly how the FIFO handles data in the following four scenarios. Could som...
While using the iis3dw sensor, I discovered that when I employed an interrupt-based polling method to read data—where, ideally, the sensor captures data, triggers an interrupt, and then the data is read—the data acquisition frequency should be around...
Split from Any accelerometer supporting >400g with integrated free-fall detection ? - this is a separate questionHi Team,Could you please suggest a suitable wireless development board that supports LSM6DSV320X, or any latest high g accelerometer sens...
I am working with the LSM6DSV320X for vibration analysis and potential crash detection applications, and I have a few questions regarding its capabilities and system integration:Is the LSM6DSV320X considered a high-end processing device? Does it supp...
In LSM6DSV16X DS13510-Rev 4 Page 8, Table lists sensor fusion performance: Question 1: are these values guaranteed over temperature and all angles, or at a particular angle and at room temperature?Question 2: without a magnetometer or GNSS heading in...
Many years ago, at ANU in third year physics, the professor provided an object and said explain and check it as a project. Let us assume that I have a SENSOR TILE.BOX pro and I follow my training and check the output of the MEMS Studio. The first st...