MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why is LSM6DSL using so much current in power-down?

Posted on June 16, 2018 at 05:12We are seeing a large current draw when the LSM6DSL is in power-down mode, or low-power mode. The current measured is roughly 120 uA. IC is wired for I2C. We have an identical setup with a LIS3DH that does not have th...

Cars Smu by Associate II
  • 2118 Views
  • 4 replies
  • 0 kudos

X-CUBE-MEMS1 Unicleo-GUI

Posted on June 18, 2018 at 13:10Hello! I have looked at video about X-CUBE-MEMS1 ( /external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3D45baO5Lxv-o%26t%3D313s ). After that, I've installed Unicleo-GUI and in tab FW Managment I don't s...

LSM330TR GYRO power_down mode

Posted on June 21, 2018 at 06:58Hi, I'm in trouble about LSM330TR gyroscope power_down mode.I'm measuring the angular velocity every 100ms and when it isn't measuring, i'd like to implement power_down mode.I wrote such a program but the gyro data is...

LV53L0X outside

Posted on June 17, 2018 at 21:30are there any settings or lenses for the LV53L0X to help it cope with high ambiant light?#lv53l0x #outside

VL53L0X_SetVcselPulsePeriod?

Posted on June 21, 2018 at 19:54is there any information of any type regarding the funktion   VL53L0X_SetVcselPulsePeriod how do i use it in other ways then what is in the API note?

Wrong result from MotionFX

Posted on June 21, 2018 at 14:18Hello,I'm trying to get run the MotionFX library using STM32L4 and SensiBLE board (which is equivalent to Nucleo-L476RG + X-Nucleo-IDB05A1 + X-Nucleo-IKS01A1 + X-Nucleo-CCA02M1).The module for the accelerometer and gy...

VL53L1 Accuracy Issue

Posted on June 19, 2018 at 14:12HiWe have interfaced VL53L1 to STM32L0 EVM board(B-L072Z-LRWAN1).We tested the sensor with a white surface and water in opaque object.The accuracy with white surface are good if the object is below 200cm.If above 200c...