cancel
Showing results for 
Search instead for 
Did you mean: 

lsm6Dsl FIFO continuous mode interrupt problem.

vladimir boretsky
Associate II
Posted on May 10, 2018 at 14:49

Hello FRIENDS!

I have problem with chip LSM6DSL using.

My purpose is use this chip in the FIFO continues mode. I would like receive interrupt from INT1 pin when FIFO full and read info from FIFO. I am working from STM32L452 processor.

I tried some chips with my dev board and I have only one chip working properly. It's mean I received rizing front interrupt from INT1 pin and I can read dates from FIFO.

Another chips not provides INTERRUPT. The contacts from microcontroller to chip was checked.

My registers set up is:

data = 0x01;

data1 = ReadLsm6ds3Register(WHO_AM_I);

if(error_status == 1)

{

acc_error_flag = 1;

return;

}

HAL_Delay(200);

//Write to FIFO_CTRL3 register. GYRO not in FIFO, Gyro -- no decimation Register adress is 0x08

data = 0x01;

error_status = WriteLsm6ds3Register(data,FIFO_CTRL3);

if(error_status == 1)

{

acc_error_flag = 1;

return;

}

HAL_Delay(200);

ReadRegister = ReadLsm6ds3Register(FIFO_CTRL3);

HAL_Delay(200);

//////////////////// FIFO CONFIGURATION //////////////////

/* Acc 104 hz */

data = 0x60; // 208Hz 0x 60 value is 416hz 0x50 208Hz 0x40 104Hz BW = 1.5KHz Register adress 0x10

error_status = WriteLsm6ds3Register(data,CTRL1_XL);

if(error_status == 1)

{

acc_error_flag = 1;

return;

}

HAL_Delay(200);

ReadRegister = ReadLsm6ds3Register(CTRL1_XL);

HAL_Delay(200);

/* Set FIFO 3rd and 4th NOT in FIFO Register number 0x09 */

data = 0;//0x01;

error_status = WriteLsm6ds3Register(data,FIFO_CTRL4);

if(error_status == 1)

{

acc_error_flag = 1;

return;

}

HAL_Delay(200);

/* Set Fifo ODR to 104Hz and Continuous mode . Register number 0x0A */

data =0x36; //FIFO continues mode

error_status = WriteLsm6ds3Register(data,FIFO_CTRL5);

if(error_status == 1)

{

acc_error_flag = 1;

return;

}

HAL_Delay(200);

ReadRegister = ReadLsm6ds3Register(FIFO_CTRL5);

HAL_Delay(200);

/* Set FIFO ODR to highest value *

if (BSP_GYRO_FIFO_Set_ODR_Value_Ext(LSM6DSL_G_0_handle, LSM6DSL_FIFO_MAX_ODR) == COMPONENT_ERROR)

{

return COMPONENT_ERROR;

}

*/

/* Set FIFO_FULL on INT1 Register number 0x0D*/

data = 0x20; //FIFO full flag on INT1

error_status = WriteLsm6ds3Register(data,INT1_CTRL);

if(error_status == 1)

{

acc_error_flag = 1;

return;

}

HAL_Delay(200);

ReadRegister = ReadLsm6ds3Register(INT1_CTRL);

HAL_Delay(200);

/* Set When the FIFO is used, the IF_INC and BDU bits of the CTRL3_C register must be equal to 1. Register number 0x12*/

data = 0x44;

error_status = WriteLsm6ds3Register(data,CTRL3_C);

if(error_status == 1)

{

acc_error_flag = 1;

return;

}

HAL_Delay(200);

ReadRegister = ReadLsm6ds3Register(CTRL3_C);

HAL_Delay(200);

What I do wrong?

Could send me proper registry init sequence and values?

Best regards.♯

#lsm6ds3 #mems #lsm6dsl
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0