cancel
Showing results for 
Search instead for 
Did you mean: 

Bluecoin power consumption - why and how to minimize?

Part Robot
Associate II
Posted on March 30, 2018 at 14:16

Hi.

I'm noticing that when using the BVLINK or MEMS software with the device paired with an iPhone the BlueCoin is using about 40-45mA. This seems a high. I'm expecting 10-20mA maximum based on other similar products I've used in the past for similar use cases. Additionally, if the power battery levels reported in the iPhone app are accurate (which I doubt since at full charge it reports alternately 97% and 80% charged), then the device appears to shutdown when the LiPo is at 20-30% capacity. This power usage is the same even if the device isn't 'doing anything' - i.e. is merely paired with the phone.

Consequently I have the following questions:

1) Does this sound reasonable/correct?

2) Is it possible to shut down all other features to conserve power?

3) Is there an ultra-low power standby mode I can activate? How do I then wake the device?

4) What other power saving measures can I take?

5) Why does the battery level switch between 80% and 97% when fully charged?

Currently my only solution is to hard shut down the device and start it up again every time I wish to use the microphones.

Specifically my use case is to press a button to record some speech and the release the button to stop recording. The battery needs to last at least a week. My space requirements allow for a LiPo up to 500mAh.

I have read the docs available at STEVAL-BCNKT01V1 - BlueCoin Starter kit - STMicroelectronics but they are insufficient. Anything more related to actually programming the BlueCoin would be gratefully received as I'm very new to this particular type of device (I've only programmed Arduinos until now).

Many thanks,

PartRobot

#bvlink #battery-life #power #bluecoin
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Andrew Neil
Super User
Posted on March 30, 2018 at 15:56

Any supporting documentation would be gratefully received

Here: 

http://www.st.com/en/evaluation-tools/steval-bcnkt01v1.html

  
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on March 30, 2018 at 15:58

Thanks but I mean supporting documentation related to the questions I have. I've read through all that and I don't see a reference to solutions for the above. I must add, however, that I don't necessarily understand all what I'm reading!

Posted on March 30, 2018 at 18:00

This might be better moved to the

https://community.st.com/community/mems-sensors-community/mems-sensors-forum

There needs to be better access to FAE and managers from the group responsible for the BlueCoin kit design.

The usual dynamic for that would be via your local ST sales and support contacts, although the expectations I think are shifting to more staff being available and responsive via 'social-media' or forum type venues. You're pushing these things into the hands of makers and engineers working out of garages/basements, not just large design groups at Apple/Nike etc with deep rosters of talent.

Kling.Brian

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 30, 2018 at 18:08

Thanks Clive. Yes, that looks to be a better place to post this. I'll do that now.

I am finding it all bit opaque, as you point out. Fortunately the code is largely self-explanatory, but the hardware/HAL stuff is very sparsely documented and fragmented. Mostly I've figured things out by looking at the source code and ending up on random forums but it's not been easy

Posted on March 30, 2018 at 19:01

Clive One wrote:

You're pushing these things into the hands of makers and engineers working out of garages/basements, not just large design groups at Apple/Nike etc with deep rosters of talent.

Indeed.

Also, the newly re-vamped 'Partner' programme now excludes small consultancies - exactly the kind of people that such enterprises would turn to for professional support ...

Kling.Brian

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on March 30, 2018 at 19:53

Well that certainly seems to be a counter-intuitive move, on the one hand you've got a push into the maker space, and to the more agile engineering of small groups or startup focused mindsets, against large slow moving corporate orientation, where small is irrelevant and tiresome, and you only want to bet on sure-things.

The easy integration and mash-up of shields and DISCO/NUCLEO boards mean people are going to try more and different things, there's less cost and more likelihood of throwing paint against a wall to see what sticks, and discarding bad solutions, or ones where the vendor just seems disengaged.

When you throw tens of thousands of low cost boards into the market you're going to need ramp your support staffing to carry that new loading, and the level of responsiveness people are accustomed too receiving, or expecting too receive, regardless of their perceived size or business penetration. Forums provide leverage, you answer one persons question, and your answer reaches a 100 or 1000 working in the same problem space.

At the end of the day this is going to be carried by individuals, like yourself, and those that can quickly parachute into to solve problems, rather than large body-shops filled with people who know next to nothing, or is as shallow as their script.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on April 03, 2018 at 09:20

I have moved this post over to MEMs and Sensors, so I'll delete the other one. I'll highlight this internally and see if we can't get some eyeballs on it!

Part Robot
Associate II
Posted on April 25, 2018 at 19:46

Anyone have any thoughts on this? Issue still remains and Bluecoin is unusable for this project until we have some details about the low power mode.

Davide G
ST Employee
Posted on May 09, 2018 at 12:44

Hi,

I’ll try to reply in order.

1) Does this sound reasonable/correct?

Both firmware examples you mentioned (BVLINK and ALLMEMS) are not optimized for Low Power and the MPU is always running at full speed, no matter what the firmware is doing. This is why you always see 40-45mA.

2) Is it possible to shut down all other features to conserve power?

Yes it is, even though STM32F446 it’s not the best choice for very low power applications (STM32L family would be the best choice).

Here there is an application note about “Using STM32F4 MCU power modes with best dynamic efficiency�.

http://www.st.com/resource/en/application_note/dm00096220.pdf

Even if it isn’t specific for the STM32446 I think it could be a good starting point.

3) Is there an ultra-low power standby mode I can activate? How do I then wake the device?

4) What other power saving measures can I take?

At chapter 5.3.3 of STM32F446 Ref Manual

http://www.st.com/resource/en/reference_manual/dm00135183.pdf

you can find the details about the different power modes.

As an example, the device could be woken up using an interrupt coming from one of the sensors (like the accelerometer) or a button.

5) Why does the battery level switch between 80% and 97% when fully charged?

Not sure at this point. This should be investigated further.