MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303AGR and int1

Posted on June 27, 2018 at 11:09With the next configuration, the INT1 don't start.Base on (https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm303agr_STdC)lsm303agr_xl_operating_mode_set(&dev_ctx_xl, LSM303AGR_XL_POWER_DOW...

Resolved! 360 degree rotation on all axis, LIS3DSH

Posted on June 21, 2018 at 00:36Hi all, I'm working with the LIS3DSH accelerometer which is the accel2 click board on the raspberry pi. I was able to get the angles of x, y, and z-axis based on the binary reading and I was also able to determine the...

0690X0000060BkZQAU.png 0690X0000060BknQAE.png

Interrupt GPIO VL53L0X

Posted on February 21, 2018 at 14:47hi,  how does the Vl53L0X ranging sensor adress the GPIO for the interrupt, i can only find a long list of register adresses in the vl53l0x_interrupt_threshold_settings.h.After initialization and calibration of th...

jonas m by Associate II
  • 3013 Views
  • 4 replies
  • 0 kudos

Why is LSM6DSL using so much current in power-down?

Posted on June 16, 2018 at 05:12We are seeing a large current draw when the LSM6DSL is in power-down mode, or low-power mode. The current measured is roughly 120 uA. IC is wired for I2C. We have an identical setup with a LIS3DH that does not have th...

Cars Smu by Associate II
  • 2219 Views
  • 4 replies
  • 0 kudos

X-CUBE-MEMS1 Unicleo-GUI

Posted on June 18, 2018 at 13:10Hello! I have looked at video about X-CUBE-MEMS1 ( /external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3D45baO5Lxv-o%26t%3D313s ). After that, I've installed Unicleo-GUI and in tab FW Managment I don't s...