MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H3LIS331DL capture drop events

I am using an H3LIS331DL accelerometer on a custom PCB. I wish to use it to attempt to capture some drop events. Using an analog accelerometer, I have seen that the drop event occurs within approximately 1-1.5 msec. Will this accelerometer be able to...

MMacL.12 by Associate
  • 1057 Views
  • 1 replies
  • 0 kudos

Using 3DoF magnetometer for position information

Our application would like to track the attitude of an object - yaw, pitch, and roll - at 500Hz update rate. The object is not moving very fast, but accuracy is important; for example, it would move through a 30 degree arc in about 1 second, and we w...

Resolved! Strange schematic for X-NUCLEO-53L1A1, I2C level shifter

Hi,X-NUCLEO-53L1A1 expansion board uses an IC (ST2329AQTR) to shift the 3.3V I2C bus lines of the MCU to a 2.8V I2C bus for the proximity sensor VL53l1x.Why are there these strange connections between the 3.3V and 2.8V bus as shown on the schematic o...

0690X000006CHmMQAW.png
JWill.12 by Associate II
  • 2189 Views
  • 4 replies
  • 0 kudos

LSM6DS33 Temperature Sensor compensates the Gyro/Accel Sensitivity?

Hi thereWe use the LSM6DS33 mems and need to have accurate gyro data. As the LSM6DS33 has an internal temp. sensor I'm wondering if the gyro/accel sensitivity is automatically corrected by the sensitivity of +16 LSB/°C?We use the FIFO continous mode ...

AKoll by Associate
  • 1317 Views
  • 2 replies
  • 0 kudos