MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Difficult to find values from

Hello ST, Am working on Steval-MK1159V1 Sensor which is interfaced through SPI to SAME51 Controller( Atmel ). I have been gone through Analysis of this Sensor. I Read LSM9DS1 Document. In Application, i read values of register which is 16 bit and mul...

kD1 by Associate II
  • 831 Views
  • 0 replies
  • 0 kudos

IddPdn specification for LIS2DE12

I am designing a product for a client and have selected the LIS2DE12 for it's low power consumption. I have measured the power consumption (standalone), with nothing connected to it to be 160uA with VDD and VDDIO both connected to 3.0V. When I remo...

WendtLabs by Associate II
  • 1638 Views
  • 4 replies
  • 0 kudos

VL53L0X spurious readings noted when kept on floor

I am using VL53L0X for distance sensing with a PMMA (acrylic) glass cover of 0.6 mm on it at an distance of 0.4 mm. When i keep the sensor on the ground and try to get the distance measurement when there is nothing but the roof in front of the sensor...

Problem with the iis328dq's data ready interrupt

I'm trying to read the data from the iis328dq using the data ready function.To do so, I wrote the CTRL_REG1 with 27h and CTRL_REG3 with 82h to have the accelerometer working in normal mode with 50 Hz of ODR. I use SPI at 25 Mbit/s to comunicate with ...

LPS22HH I3C Address Assignment Collision

I'm working on a new design requiring four pressure sensors. The LPS22HH only allows two I2C address's through pin 5. Rather then increase complexity by putting all four on SPI I wanted to see if I could use the I3C bus capability. The datasheet refe...

STEVAL-MKI015V1 with STEVAL-MKI109V3 and Unico 7.0.0.0

I'm trying to evaluate STEVAL-MKI015V1 with STEVAL-MKI109V3 and Unico 7.0.0.0. The device appears in the selection menu, but I got the error "Device is not supported by the motherboard". I successfully completed the firmware upgrade through DFU (curr...

SROSS by Associate
  • 1007 Views
  • 1 replies
  • 0 kudos