Hi, currently, lis3dh is running well with IA1 function, but if i want to change some config, such as CTRL_REG1(20h) for change target axis INT1_CFG(30h) for target axis and direction change INT1_THS(32h) fo...
Hi, from Data sheet, i saw section 3.5, it says no need to further calibration but when i check output data from register 28-2D, the value is variety time to time , it has variety range for +- 20 ~ +-40, is it correct? or we should do calib...
Hi, my setting is 10 bit with normal mode, with FS = +-2g, ODR = 100Hz and i've measure for 5 minutes with 5 times, the average of conversion is 1010 mg, point to ground regardsGary
Hi thanks for reply, i guess the unit should be mg output_x = (value from register 28-29) * sensitivity the sensitivity is define as "#define SENSITIVITY_2G 1 /** mg/LSB */" i also do some calculate with sqrt(output_x^2 + output_y^2 +...