Skip to main content
JWill.12
Associate
October 30, 2018
Solved

Strange schematic for X-NUCLEO-53L1A1, I2C level shifter

  • October 30, 2018
  • 4 replies
  • 2213 views

Hi,

X-NUCLEO-53L1A1 expansion board uses an IC (ST2329AQTR) to shift the 3.3V I2C bus lines of the MCU to a 2.8V I2C bus for the proximity sensor VL53l1x.

Why are there these strange connections between the 3.3V and 2.8V bus as shown on the schematic of the X-NUCLEO-53L1A1 (see attached file) ?

0690X000006CHmMQAW.png 

Thanks,

Jeremie

This topic has been closed for replies.
Best answer by Miroslav BATEK

I think the schematic is not correct, the 3.3V and 2.8V buses cannot be connect together (shorted).

Most probably solder bridges are missing in the schematic.

4 replies

ST Employee
October 30, 2018

The nominal power supply voltage for VL53I1x is 2.8 V.

JWill.12
JWill.12Author
Associate
October 30, 2018

I'm aware of that. My question is about the i2c level shifter, from 3.3 to 2.8V. Why are the 2 bus connected? What's the point of the level shifter in that case?

Miroslav BATEKBest answer
ST Employee
October 30, 2018

I think the schematic is not correct, the 3.3V and 2.8V buses cannot be connect together (shorted).

Most probably solder bridges are missing in the schematic.

JWill.12
JWill.12Author
Associate
October 30, 2018

Ok, we agree on that.

Thanks