MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 Timestamp read in FIFO issue

I have a LSM6DS3 sensor connected to a MCU by SPI. My goal is to fill the FIFO buffer with the following sets of data: Gx, Gy, Gz, XLx, XLy, XLz, Ts, Pd. I am using a watermark to generate an interrupt once a specific FIFO level is reached. Furthermo...

Output data from LSM6DS3 appnote doesn't make sense

We're evaluating the LSM6DS3. Its appnote (D027415 Rev 5) has table 20 on page 39, "Output data registers content vs. angular rate (FS_G = +/- 250dps)". Zero is zero, no problem there. The other examples are 100 and 200 dps. Let's use the positive va...

LIS3DSH. Data for X, Y, Z does not change.

Started working with LIS302DL. Then took the LIS3DSH. The program is the same. After starting LIS3DSH, it gives correct readings along the axes, but after a few seconds of work, the data becomes permanent. The time to failure varies from a few second...

progs_sp by Associate II
  • 1248 Views
  • 2 replies
  • 0 kudos

LSM6DSO SPI communication problem

Good morning,I am trying to read the WHO_AM_I register from LSM6DSO, but it doesn't respond as needed. I will attach a picture from signal analyzer (D0 is CS, D1 is CLK, D2 is MISO, D3 is MOSI). It looks like its respond is 0x50 instead of 0x6C. What...

Which is g calibration value?

Hi to all, which is factory calibration value for g for MEMS accelerometers?Is this value the same for all accelerometers (I suppose)?Thanks.

mbertoni by Associate II
  • 2124 Views
  • 4 replies
  • 0 kudos

SensorTile Drivers and Implementation

Posted on March 20, 2018 at 11:21Hello All,I am having a a bit of an issue working with my SensorTile kit. I am able to get the demo apps working and so on, but I now want to start on my own project.For the moment I have just tried to set the MCU up...

dylan by Associate III
  • 2730 Views
  • 5 replies
  • 2 kudos

BMI160 pins 2 and 3 - safe to connect to ground?

The BMI160 spec sheet says pins 2 and 3 are high impedance when the secondary I2C interface is not being used. The spec sheet also *implies* that the secondary I2C interface defaults to disabled upon a power cycle. The question is, can pins 2 and 3 b...