MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! H3LIS331DL: Threshold levels

I have the FS bits set for +/-100g scale.The accel data is a 12-bit signed value, meaning each bit represents 0.049g.The threshold registers however is only a 7-bit value. From what I understand, this is to be an unsigned magnitude level, representi...

RDyla by Associate II
  • 1724 Views
  • 3 replies
  • 0 kudos

How to use pdm to pcm conversion library?

I am working on a project where I need to calculate the ambient noise in a given environment in decibels, for that purpose I am using st microelectronics's MP34DT01-M microphone which has an digital PDM output. From the stm application notes I got t...

SHire by Associate
  • 1600 Views
  • 2 replies
  • 0 kudos

IIS2DH sensing Die Location

Where in the 2x2 package is the sensing die for the 3 axis located? Is it dead center? A technical answer as accurate as possible would be best. And if there is some known manufacturing variance ​of this location. ​T​hanks

Interrupt generation for activity event

Hello,I have configured LIS2DH12 to generate interrupt on INT2 pin on activity as well as a strong impact using the register values as follows:CTRL_REG1 - 0x37CTRL_REG2 - 0x00CTRL_REG3 - 0x40CTRL_REG4 - 0x88CTRL_REG5 - 0x0ACTRL_REG6 - 0x28INT1_THS - ...

AB.4 by Associate II
  • 703 Views
  • 0 replies
  • 0 kudos

LSM9DS1 magnetic sensitivity

Posted on July 10, 2018 at 16:40The magnetic sensitivity for the LSM9DS1 is 0.14 mguass/LSB on its most sensitive range.  The LIS2MDL is 1.5 mguass/LSB.  Is the LSM9DS1 really 10X more sensitive?  If so, it would seem the best choice for application...

A3G4250 gyroscoppe questions ?

Dear ST Members,How can convert the register output X,Y,Z to dps ? I read on datasheet , the range is +/- 245 dps. What's "dps" ?Best regards,Bianchi

looking for Car detection Sensor

Hi ,I am using 3 axis Magnetometer Sensor(LIS3MDL) Sensor for Car detection. but issues is some time it's not working. please suggest me any other low power proximity for detecting car.

VL53L1X can't connect with MCBSTM32 Evaluation Board

Hello I have a MCBSTM32F103 Evaluation Board but I can't connect it with the VL53L1X Satel. I use Keil, first I have include the API to use the functions. Then I use the VL53L1X expansion board Code and modify the platform.c and the main. If I compil...

ST1 by Associate
  • 830 Views
  • 1 replies
  • 0 kudos