MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HTS221 with Half duplex SPI

Hello,I'm currently programing a self designed sensor node with a HTS221. I've decided to use SPI to communicate with it (SPI half-duplex master)Here are the settings:static void MX_SPI2_Init(void) {   /* USER CODE BEGIN SPI2_Init 0 */   /* USER ...

SSchm.16 by Associate
  • 1682 Views
  • 3 replies
  • 0 kudos

Unicleo-GUI not starting

Hi,i've installed Unicleo-GUI to test X-NUCLEO-IKS01A2 MEMS but the GUI is not starting. In addition i have installed latest Qt5+MinGW64, AlgoBuilder and STM32CubeMX with Firmwares. I see the Unicleo-GUI.exe popup in Windows Process Explorer and afte...

ToolV by Associate II
  • 1035 Views
  • 1 replies
  • 0 kudos

Resolved! Lowest power mode for accelerometer application in STM32L4 ?

Hi, I wanna use the lowest power mode possible for my stm32l432kc. I want MCU to wakeup on accelerometer motion (which is possible since the accel generate interrupt on motion). I've read in MCU appnopte AN4621(page 13) that i2c is detected only in s...

Resolved! How do I save the temperature in a log from the LIS3DH through Unico?

I have a LIS3DH sensor and Unico 7 in my computer and I am using the evaluation board MKI109V3. The thing is that I want to save the temperature data (measured by the Embedded Temperature sensor inside the LIS3DH) in a log file and with Unico this is...

VGuer by Associate II
  • 3509 Views
  • 7 replies
  • 0 kudos

Can someone with internal knowledge confirm that the LIS3DSH in I2C mode never drives the SCL line low and that a standard "single master push-pull SCL" can be used in combination with the bidirectional SDA line.

The LIS3DSH datasheet contains the following text (not very clear):"If a receiver can’t receive another complete byte of data until it has performed some other function, it can hold the clock line, SCL LOW, to force the transmitter into a wait state....

LeiNie by Associate
  • 869 Views
  • 0 replies
  • 0 kudos

What does COUNTER_BDR_REG1?

Hi,I am using LSM6DSO and I am trying to implement the FIFO feature. I am reading from here (https://www.st.com/content/ccc/resource/technical/document/application_note/group0/56/95/d6/a1/34/4c/49/6d/DM00517282/files/DM00517282.pdf/jcr:content/transl...

X-Nucleo expansion board for LSM6DSO?

Hi, is ST planning to release new version of the X-NUCLEO-IKS01A2 sensor expansion board with the newest recently released sensors? I would like to interface LSM6DSO with NUCLEO-L4. Tks

f87 by Associate II
  • 734 Views
  • 0 replies
  • 0 kudos

LSM6DSO no interrupt

I have a LSM6DSO and I want to test it with the data ready interrupt, but I don't get any. I am using a logic analyzer to monitor the interrupt.The registers that I set are:0x18 with value 0x010x0B with value 0x010x10 with value 0x400x0D with value 0...