cancel
Showing results for 
Search instead for 
Did you mean: 

High standby current of LIS3MDL

AChan.5
Associate

The static current of LIS3MDL is 0.2mA while the pin is connect to ground serial with 10K resistor, if this pin is floating, the current 0.07mA.

The sensor is communication with Noridic nrf52 MCU via I2C. Please advise the appropriate connected for the pin SDO/SA1. 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Miroslav BATEK
ST Employee

SDO/SA1 pin defines the I2C address.

If you have a freedom to choose the I2C address connect this pin to VDD_IO.

The pin can be connected to GND as well but the current consumption will be higher due to internal pull-up.

AChan.5
Associate

How about LSM6DS33, it is work togehter with LIS3MDL, at this moment, the SDO/SA0 pin is connect to Ground.

Miroslav BATEK
ST Employee

For LSM6DS33 the pull-up on SA0 pin is disabled by default, so you can connect it to VDDIO or GND without impact on current consumption.