MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1´S API implementation for Microchip devices: Doubts.

Hi friends,I´m trying to include a Vl53l1 in my project. I am working with a PIC32MX440 microntroller.I have filled with correct functions in the files vl53l1_platfom.h and .c to use the APIs with my hardware.The commication with the sensor is right...

H3LIS331DL sensor readings do not change

I'm using the STEVAL-MKI153V1 evalulation board together with a Nucleo F443RE board and the STM reference driver implementation from github.The code is basically the read_simple.c example provided by STM adapted to mbed.I've checked the I²C communica...

NLieb by Associate II
  • 1044 Views
  • 1 replies
  • 0 kudos

Device Tree Initialization of RTC M41T80 Clock-Provider

Hi everyone,we are using an M41T80 RTC on our custom linux board. This RTC has a CLK-OUT feature which is per default to ON and 32kHz. We have another chip wired and depending to that clock signal.On kernel version 4.1.15 there was no feature to enab...

LSM6DS3 3D Gyroscope best ODR Selection

Hello all,We have interfaced LSM6DS3 with a wireless microcontroller by I2C for .I want to know how do I select the best ODR value?Is there any standard methods for selecting ODR?According to datasheet I found that if ODR is high the current consumpt...

VDhan by Associate II
  • 3819 Views
  • 5 replies
  • 0 kudos

LIS2DE12 - What is low-power mode

Hi,Can some one explain what is low power mode. It is mentioned in page 45 in the data sheet. But no where it is explained. I would like it to work in low power mode and wake up on certain condition (also cause INTERRUPT) and go back to low power mod...

jonfs2000 by Associate II
  • 1264 Views
  • 1 replies
  • 0 kudos

LIS2DE12: Movement detection over interrupt question

Hello there,I have a question about this sensor. I'll be using it as a low-power device on a PIC, which is most of the time in sleep mode, and will wake up on interrupts from various devices. I want to configure this sensor so it will notify the PIC ...

Simon_ by Associate
  • 2379 Views
  • 1 replies
  • 1 kudos