MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help with programming the STM32 STEVAL-STLCS01V1 (with the STEVAL-STLKT01V1 Sensor development kit) using Arduino Uno sketch IDE.

I want to program the mcu STM32 STEVAL-STLCS01V1. I have the STEVAL-STLKT01V1 Sensor development kit and i've read that i can mount the STLCX01V1 on the Arduino Uno board, mount the STEVAL-STLCS01V1 on the STLCX01V1 board. and then use the Arduino sk...

RFink by Associate II
  • 988 Views
  • 0 replies
  • 0 kudos

Need help getting initialized with MSP430F5529 to lsm303agr using STMems_Standard_C_Divers

 P4SEL |= 0x06;              // Assign I2C pins P4.1, P4.2 to USCI_B1 UCB1CTL1 |= UCSWRST;           // Enable SW reset UCB1CTL0 = UCMST + UCMODE_3 + UCSYNC;   // I2C Master, synchronous mode UCB1CTL1 = UCSSEL_2 + UCSWRST;      // Use SMCLK UCB1BR0 =...

JBonn by Associate III
  • 919 Views
  • 1 replies
  • 0 kudos

Is it possible to change the STEVAL-IDP005V1-GUI software files?

Hello everyone,I am conducting some tests with the STEVAL-BFA001V1B and STEVAL-IDP004V1 evaluation kit together with the STEVAL-IDP005V1 GUI software available on STSW-BFA001V1.But I need to make some changes in the STEVAL-IDP005V1-GUI software, the ...

Hertzing by Associate II
  • 1679 Views
  • 4 replies
  • 0 kudos

Resolved! STEVAL-MKI109V3 DfuSe update issue, no available DFU Device

Hello, I installed the latest driver version Unico 8.0.0. Now my board is shown in the decive manager.Ready to use.. Everything looks good.Now I am trying to update the FW in the STEVAL-MKI109V3 board. First I pressed the BT2 Button and pluged the US...

Chris0815 by Associate II
  • 1416 Views
  • 2 replies
  • 0 kudos

Generate Interrupt on horizontal rotation using LIS3DH

Hi,I have a jar lid which is equipped with LIS3DH accelerometer. The accelerometer is placed in the PCB such that the top layer of LIS3DH will face the sky in normal position. The jar has a groove for holding the lid and we need to put the lid in th...

IThom.5 by Associate II
  • 2437 Views
  • 5 replies
  • 0 kudos

LIS2DH12TR 1. Calibration 2.sleep mode and wake-up mode detail explanation & 3.example code for interfacing with the CC1310 (SCS and CSS)

Hi,I have couple of question on LIS2DH12TR .I'm trying to interface with CC1310 Custom Board.1. As per the data sheet it says it doesn't need any manual calibration since factory calibration already done.( Previously have used MPU6050 didn't know m...

LN by Associate II
  • 1124 Views
  • 1 replies
  • 0 kudos