MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Lis3dh reading not repeatable/stable

HiWe are developing a project in which we are using LIS3DH to calculate the angle and based on that angle we stop/start an actuator.The sensor is mounted on a PCB which is aligned along x axis i.e. when stationary the acceleration in x axis is 1g * 9...

lis3dh.png
pthakkar by Associate II
  • 1131 Views
  • 2 replies
  • 0 kudos

Resolved! LPF2 on IIS3DWB and anti-alias

I use IIS3DWB with no LPF2 enabled, and I understand the Frequency response shown in Figure 13 at page 20 of the datasheet.I know that I can enable low-pass LPF2 filter, but from the same graph I don't understand if this filter can be enabled as a ha...

vix by Associate II
  • 3634 Views
  • 6 replies
  • 0 kudos

Resolved! MEMS Studio Not Detecting STEVAL-MKI109D

I followed 'STEVAL-MKI109D Professional MEMS Tool motherboard for MEMS adapter boards' and installed MEMS Studio.I then placed STEVAL-MKI250KA on STEVAL-MKI109D by following UM3420 and AN6173.  When I boot MEMS Studio, it just does not recognise the ...

no conn.png
seanjm by Associate
  • 1090 Views
  • 1 replies
  • 1 kudos

Resolved! Query about MDRDY Signal Configuration in LSM6DSO16IS MODE2

I am working with the LSM6DSO16IS in MODE2 configuration with ISPU enabled. I have some questions regarding the MDRDY (Master Data Ready) signal:1. How is the MDRDY signal handled in MODE2 when using the master I2C interface with external sensors?2. ...

seanfan by Associate
  • 896 Views
  • 1 replies
  • 0 kudos

Unable to read the mic value IMP34DT05TR

We are interfacing the IMP34DT05TR microphone with the STM32F423ZHJ6 microcontroller. I have attached the schematic for reference. However, we are unable to read the microphone data on our custom board, as we always get a NULL value in the output. La...

srinithi_09_0-1743055976941.png

Stream sensortile box pro data via USB into Matlab

Hello, I have the sensortile box pro. I have used the algobuilder in the MEMS-studio to configure various data outputs (Acc, Gyr, RotationVector 6x). The sensortile isplugged in with USB. I can see those data coming into the MEMS-studio algobuilder e...

Gawa by Associate
  • 1189 Views
  • 2 replies
  • 2 kudos