MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ISM330DLC : How to properly set FIFO

Hi,I am really new to this sensor and I was able to get the polling mode working.I am planning for full 6.6k odr rate and FIFO samples can be 256 when INT1 should be triggered or whenever possible so I can use FIFO .I am really confused with the orde...

AmrithHN by Associate III
  • 1119 Views
  • 1 replies
  • 0 kudos

data ready interrupt lsm6dsl

Posted on June 09, 2017 at 16:37Hello everyone,I Would like read the lsm6dsl data by interrupt using the pin int1 on the sensor.I configured the accelerometer ODR to 104 HzAnd i set up registers as follow : - Control_3C (0x12) =  64 (Data updated on...

Can't connect the SensorTile with Raspberry pi

Hi,I want connect my SensorTile box with my Raspberry pi. For this, I use example_ble_1.py, but every time when i try to connect the devices then one of the given errors occur:guest@raspberrypi:~ $ sudo python3 example_ble_1.py##################BlueS...

Milan127 by Associate II
  • 2669 Views
  • 4 replies
  • 0 kudos

Resolved! Identification IMU

I have a problem with identifying the sensor type from the marking on the housing. One is LSM6DSO32XTR and the other is ASM330LHHXTR. Unfortunately they came in a bag without a description on the label. One is marked T3 [QR code] 233 and the other LC...

Nairh by Associate II
  • 3398 Views
  • 8 replies
  • 2 kudos

Resolved! LSM6DSV on STEVAL MKI239A with Nucleo board via SPI not working

helloI've been trying to use the LSM6DSV on it's steval-mki239a board with a nucleo board (nucleo-l476rg) via SPI and the lsm6dsv is not answering whatever the configuration of my SPI is.The sensor is fine since it work with the steval-mki109v3 board...

Eddess_0-1743493087888.png Eddess_1-1743495078971.png Eddess_2-1743495176541.png Eddess_5-1743495442778.png
Eddess by Associate II
  • 932 Views
  • 1 replies
  • 1 kudos

LIS2DH12 HOWTO Convert Register value to mg value

Hi,  I am using the LIS2DH12 to interrupt me on an inertial wake.  I am running in Low Power mode with a scale of 4G.  After verifying that the X axis produced the force that caused the interrupt I read the X_OUT_L and X_OUT_H registers to get the 2'...

DPatt.2 by Associate II
  • 993 Views
  • 4 replies
  • 2 kudos