Hello everybody!Sorry for the question but i am in need of help.I use STM32CubeIDE 1.5.1 with stm32 discovery f407g to manage an exyernal adc ADS1118.ADC works well with Arduino, but unfortunately I can't get it to work with discovery.... /* USER COD...
Hello,i use iis2dh (STEVAL-MKI168V1) on Arduino Due through spi.unfortunately, the y axis does not respond (I tried 3 development boards!).if instead use STEVAL-MKI135V1 board the same firmware works.could someone help me?best regards,Francesco
in one case I use a lib made by me, in the other case i use SparkFunLIS3DH lib.When I use SparkFunLIS3DH lib on STEVAL-MKI135V1 board no I have problems on the three axes. When I use SparkFunLIS3DH lib on STEVAL-MKI168V1 board only the y axis is fi...