MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DSH SPI address increment problem

I am using an ST Micro MCU via SPI to the LIS3DSH to read x,y,z data(using CubeMX HAL). I can read in single byte mode fine but the multi byte access bit in Control register 6 has no effect. I have tried Control register 6 : ADD_INC disabled or enab...

PVall by Associate II
  • 1246 Views
  • 2 replies
  • 0 kudos

LSM6DSM loses its configuration.

LSM6DSM loses its configuration when another chip in the board is turned on. SIMO pin goes up for 1.5ms when it happens, with a voltage of 2.2V even though the accelerometer is fed with a 2.8V supply voltage. I do not see a glitch below 1.8V which co...

SRezk by Associate II
  • 1129 Views
  • 1 replies
  • 0 kudos

LIS3DH ADC1 input troubleshooting

I've implemented a new low power design using LIS3DH, and I had in mind to use ADC1 input to monitor the battery voltage and ADC3 to monitor temperature.I succeed to properly read all three accelerometers axis as well as temperature. On the ADC1 inpu...

CALAY by Associate II
  • 1991 Views
  • 3 replies
  • 0 kudos

Question about LIS3DH FIFO operation

Hi,I want to configure the LIS3DH working with FIFO mode and OVERRUN interrupt on INT1. So, once the interrupt occur, MCU will read all data from FIFO. by reading the datasheet, I am a little bit confused for FIFO overrun behavior. On the page 22 of ...

jeffz by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

Send data from sensortile kit to raspberry pi

Can anyone tell how can we send the sensor data from sensortile sensor kit to raspberry pi through ble. We have tried the method of pairing but it is not pairing with raspberry pi.

SKris.13 by Associate
  • 1302 Views
  • 1 replies
  • 0 kudos

How can I get the quaternion matrix Q directly from LSM6DSO?

I download the document from your website, it shows how to rotate the coordinate, while the function it uses directly get the quaternion matrix Q which I cannot read from the board, can some one told me how to get this Q data? Attached is the documen...

Sunny.Q by Associate II
  • 3356 Views
  • 3 replies
  • 0 kudos

Configure LIS3DSH state machine to detect angle change?

I've used the LIS3DSH state machine to set the INT1 interrupt high when a certain acceleration threshold is exceeded. However, I'd like to use the state machine to detect a change in orientation.For example, I'd like it to set the interrupt high whe...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.