MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303AGR heading angle calculation problems.

Hi,I'm trying to get the heading direction from the compass of LSM303AGR, I'm getting the X,Y,Z data and configured the compass and the accelerometer.I just preform a atan2(y,x) function and not using any filtering or compensations. I wanted to see d...

netanelu by Associate III
  • 1036 Views
  • 0 replies
  • 0 kudos

Hi I´m working with LI2DTW12 acelerometer chip. I trying to configure the sensor to generate an interruption in the INT_1 when the device detect an aceleration in the Z axis. Could you help me with the register configuration?

Hi I´m working with LI2DTW12 acelerometer chip. I trying to configure the sensor to generate an interruption in the INT_1 when the device detect an aceleration in the Z axis. I have configure the device registers in the following way:uint8 array_regi...

JFern.2 by Associate II
  • 2929 Views
  • 7 replies
  • 0 kudos

HTS221 T0_OUT & T1_OUT = 0

Currently having some issues reading the temperature correctly from the HTS221 sensor.The Coefficients read as follows.H0_T0_OUT = 0x5246H0_rH_x2 = 0x57H1_T0_OUT = 0x0000H1_rH_x2 = 0x95T0_OUT = 0x0000T0_degC_x8 = 0x27T1/T0 MSB = 0x4BT1_OUT = 0x0000T1...

MTrav.19 by Associate
  • 1068 Views
  • 1 replies
  • 0 kudos

LPS33HW accuracy question

Hello,I have a question related to accuracy of this sensor see attachmentFrom the datasheet I can read that the accuracy over temperature is +/2.5hPa. Did I correctly understand that the accuracy of the sensor can change within this range only in thi...

I am working on using an STM32L4 as a SMBus host to communicate to a battery monitor IC with many different registers. Using cubeMX and HAL to generate my code, I am having trouble understanding the functions and variables. Help!

From what I understand, the slave device I want to communicate with has many addressed registers than I need to specify in addition to the slave device's address. If the slave device's address is 0x16, and the registers I need to read on that device ...

JLand.8 by Associate
  • 990 Views
  • 0 replies
  • 0 kudos

SensorTile.box #6: Why should I use the ST.box Expert mode

Why should one need something more, if a lot of everyday-life applications are already available by default as examples? Different reasons, indeed:Power optimization: Individual sensors can be activated or shut down to enable only the required sensor...

IIS2MDCTR temperature rating.

Please present the junction temperature rating of IIS2MDCTR,Is it generally the same as the storage temperature?

HTaka.8 by Associate
  • 1117 Views
  • 1 replies
  • 0 kudos

Resolved! LSM9DS1 Temperature

HI,I've problems on the temperature detected by the LSM9DS1. I used the "Unico" software to configure the Acc/Gyro and the Magnetometer, in particular I used the "Easy configuration button".I read the temperature (Unico page Acc/Gyro Registers) from ...

HTS221 water resistance

The HTS221 can handle condensation, according to the data sheet.According to that, I understand that water will not damage the sensor.(I refer to the sensing area on top, to the contacts on the bottom.)Is this correct?

GShim by Associate II
  • 1600 Views
  • 4 replies
  • 0 kudos