What configuration is required for disabling Tap Function of LSM6DSM accelerometer + gyroscope sensor?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-05 2:08 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-05 2:50 AM
Hi @girish ghadage​ , according to AN4987 (p. 44) in order to enable the single-tap and double-tap recognition functions it is necessary to set the INTERRUPTS_ENABLE bit in TAP_CFG register to 1. So, to disable the same function the same bit must be set to 0. (Btw, consider it is disabled by default). Did I correctly understood your question? Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-05 4:04 AM
Thank you for your help,
Yes you did understood the question correctly.
Issue is i have tried doing it both ways by setting the TAP_CFG bit to 0 and by leaving it to default. But when i test it, i am able to start and stop the sensor readings by tap on sensor.
I'am sharing the configuration settings i have uploaded,
sendCommand(0x10,0x3C,50); //Linear Acceleration Control
sendCommand(0x11,0x00,50); //Angular Rate Control Register
sendCommand(0x12,0x0C,50); //Control Reg
sendCommand(0x13,0x02,50); //Control Reg
sendCommand(0x14,0x20,50); //Control Reg
sendCommand(0x15,0x60,50); //Control Reg
sendCommand(0x58,0x00,50); //TAP_Cfg
also i have only need the accelerometer reading so i have disabled the angular data rate.