MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Configuration of MKI109V3, Unico, and MKI197V1

I am attempting to evaluate the LSM6DSOX IMU using the combination of MKI109V3, MKI971V1, and Unico.This is the same combination shown in several of ST's YouTube videosAll of the products are new and have not previously been installed or used.I have ...

0690X000009juuLQAQ.png 0690X000009juuQQAQ.png 0690X000009juv9QAA.png
ARenn.12 by Associate
  • 1019 Views
  • 2 replies
  • 1 kudos

SensorTile.box #5: From Entry-level to Expert mode

Till now, the described application are already-packed apps that can be simply downloaded on the Sensortile.box with just a click. Expert mode allows you to create your own application/algorithm by using Expert View in ST BLE Sensor application. We ...

0690X000009jxDAQAY.png

Resolved! LSM303AGR return only zeros

It's returning ack on the i2c on every command , and i'm getting an error if it's not the correct address.I'm attaching image from the scope of the i2c commands and responses.The configuration done first and then I'm reading the temperature that it a...

netanelu by Associate III
  • 3554 Views
  • 4 replies
  • 0 kudos

How should data ready output be configured for LIS2MDL.

I've tried to use LIS2MDL with interrupts without success.What needs to be done, and does it work with continuous mode?It looks (by the data sheet) like enabling the DRDY (bit 0 in CFG_REG_C) would be enough, but seems not.It looks like DRDY is not a...

SensorTile.box #3: A small, portable weather station

The first example application we see is the Barometer. It's on of the simplest applications because it consists only of Inputs (the Sensors) and one Output (stream to BLE). No operations (called in this case "functions") are performed on the data in ...

0690X000009jGhlQAE.png

HTS221 temperature stuck at 35C and unreliable humidity measurement

Hi there,I managed to solder about 20 HTS221 on my custom board using a small oven, some boards have a correct temperature and humidity measurement, but others are out of luck.issue 1:temperature stuck around 35C, in my room at 24c, changes on the te...

0690X000009jKQeQAM.png
JISEA by Associate
  • 1350 Views
  • 1 replies
  • 0 kudos

LIS3DH drift over time

HelloI was asked to build a device which will determine if a box is in either of the three following states: perpendicular to ground, tilted forwards (10° or more), tilted backwards (10° or more). I am attaching a simple drawing for visualization of ...