MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to communicated with STEVAL-MKI110v1 using SPI?

Hi,I am using Freedom K64F microcontroller, Kinetis Design Studio 3.2 IDE, and MQX4.2 RTOS for my project. I haven't been able to read a register correctly from the ais328dq accelerometer using SPI. I have verified with a logic analyzer that the cloc...

DLim.16 by Associate II
  • 1697 Views
  • 3 replies
  • 0 kudos

Regarding steval-mki176v1 LSM6DS3H questions are about 1) specs of the internal clock, 2) LED availability. See Details.

Regarding steval-mki176v1 LSM6DS3H :1) What are the specs of the internal clock for the gyro if you were spec-ing it like a crystal? What is the drift and drift with temperature?2) Does it have an LED to show bus activity when querying the gyro or ac...

Roumen K by Associate II
  • 3092 Views
  • 5 replies
  • 0 kudos

Both INT1 and INT2 for tilt and free fall by LIS3DH?

i m using LIS3dh accelerometer. Now i worked with 2g tilt sensor by using INT1.Now i want to add a feature like free fall by INT2.Is it possible to do both on different interrupts?If its so plz share me the registers value.

How to remove Gravity factor from Accelerometer readings .

 I am using the industrial IIS2DH accelerometer in my vibration analysis product. I need only pure acceleration values in all directions. So at any state if the device is stable (or in constant speed), it should give (0.0,0.0,0.0) roughly.

Not outputting data

My LIS3DH is not outputting any data, its displaying a value of 127, any idea why

RNata.15 by Associate II
  • 719 Views
  • 0 replies
  • 0 kudos

LIS3DSH no output data

Hi all,I'm trying to work with the LIS3DSH but i'm not getting any output data.I have verified the SPI is working, I can write to and read back numbers from the registers so I know they are getting set correctly. I'm using the initialisation code bel...

Use MEMS microphone to record audio with STM32F1 MCU

Hi,I'm sorry if i'm asking anyhting newbie. I want to use an STM32 MCU to build a voice recorde application. The data is acquired by a mic and stored in SD Car which connects via SPI with MCU. However, I've some doubts about my application.Since I ne...

MAndr.233 by Associate III
  • 2357 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.