MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS27HHW Pick&Place and conformal coating

I'm trying to use the LPS27HHW in a 1 gram wildlife tracking device (water resistance required) and am wondering (a) how pick&place is supposed to pick up the sensor, and (b) how I can apply automated spray conformal coating to the board. I would hav...

tve by Associate II
  • 2888 Views
  • 5 replies
  • 1 kudos

LIS2DH12TR Dimension Discrepancy

Hello, We received LIS2DH12TR bought from distributor source with full label and full lot code.Our QC team checked with measuring equipment, and we found the height is above the max 1.0mm. Is it considered normal phenomenon?   Referring to photo atta...

LWU.31 by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

Resolved! STHS34PF80TR INT pin Source / Sink capability?

Greetings - what are the recommended maximum current ratings for the INT pin in either Push-Pull or Open-Drain? And FWIW, I was really surprised NOT to find this published in the datasheet...TIA,-Terry

TPhil.3 by Associate II
  • 878 Views
  • 1 replies
  • 0 kudos

LSM6dSOX_MLC

Hi All,I am currently working on a health tracker/monitor project that utilizes the LSM6DSOX sensor, interfaced with the nRF5340 platform and running Zephyr. So far, I have successfully implemented tilt and tap detection features.As the next step in ...

Resolved! Sensor Tile Box Pro connection problems with pc

Hello, community! I recently purchased the SensorTile Box Pro to conduct various educational experiments. It connects via Bluetooth to my phone, but when I try to connect it to my laptop using the MEMS STUDIO application, it does not work via either ...

Ats6 by Associate
  • 1771 Views
  • 2 replies
  • 2 kudos

ISM330DLC : How to properly set FIFO

Hi,I am really new to this sensor and I was able to get the polling mode working.I am planning for full 6.6k odr rate and FIFO samples can be 256 when INT1 should be triggered or whenever possible so I can use FIFO .I am really confused with the orde...

AmrithHN by Associate III
  • 1113 Views
  • 1 replies
  • 0 kudos

data ready interrupt lsm6dsl

Posted on June 09, 2017 at 16:37Hello everyone,I Would like read the lsm6dsl data by interrupt using the pin int1 on the sensor.I configured the accelerometer ODR to 104 HzAnd i set up registers as follow : - Control_3C (0x12) =  64 (Data updated on...

Can't connect the SensorTile with Raspberry pi

Hi,I want connect my SensorTile box with my Raspberry pi. For this, I use example_ble_1.py, but every time when i try to connect the devices then one of the given errors occur:guest@raspberrypi:~ $ sudo python3 example_ble_1.py##################BlueS...

Milan127 by Associate II
  • 2663 Views
  • 4 replies
  • 0 kudos