cancel
Showing results for 
Search instead for 
Did you mean: 

QVAR Sensor - LSM6DSV16X

marshouse
Associate II

Is it possible to check the electrical activity of an AC power cable using Qvar functionality. 

What type of electrode to be used? What type of input circuitry needs to be designed (input impedance and filtering)?

 

 

 

2 REPLIES 2
henrywill12
Associate

Yes, it's possible to detect electrical activity in an AC power cable noninvasively using Qvar functionality as described in ST's AN5755. The Qvar sensor can sense electrostatic charge variations when electrodes are placed near the cable's outer insulation. The electrodes, typically made of conductive material, should be placed close but not touching the cable.

For the input circuitry, high impedance (megaohms range) is required to prevent signal interference, along with filtering to eliminate noise, focusing on the AC signal's frequency (50/60 Hz)

Is there any criteria for dimensions of the foil that matters for this use-case?