2024-10-17 1:40 AM
Hi,
I am currently using a STM32L476 with a LIS2MDL, I need to apply a calibration along only 1 axis for the magnetometer, as the system can not be rotated along the others axis.
I was wondering if there is ready made solution/library to do it?
Thank you in advance for the help or any ints
2024-10-23 2:48 AM
Hi @VDVL ,
Have you already looked at MotionFX library?
2024-10-23 7:06 AM
Yes, I use this library to fuse the datas from an IMU and the magnetometer (LIS2MDL).
The library propose "MotionFX_MagCal_run" function to calibrate the magnetometer, but (tell me if I'm wrong), it require to move the magnetometer around the 3 axis completely, if I rotate the magnetometer around only one axis (the only degree of freedom i have) it doesn't give any value.
in addition it perform only hard iron calibration, and I would also need to perform a soft iron calibration (still around one axis).
Thanks for the hints