MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! L3GD20H Wrong I2C Address

Posted on March 25, 2016 at 01:52I've got a board with a Gyro (L3GD20H) and Accel/Mag (LSM303D).  I'm interfacing with the sensors using I2C.  I can communicate with the Accel/Mag without issues.  However, the Gyro is showing up at (7bit) address 0x...

acsmith by Associate
  • 3487 Views
  • 3 replies
  • 0 kudos

How to read MLC features on LSM6DSOX?

Since LSM6DSOX can calculate some statistics on the raw data, like mean and standard deviation I would like to use this capability and read and send this data to the host app on the PC. I do not need any classifier functionality for my use case and j...

Rita Ch. by Associate II
  • 770 Views
  • 0 replies
  • 0 kudos

unable to send LIS2DW12 sensor in to sleep

Hi,we are using in our current product LIS2DW12 sensor, but we trying to send sleep accelerometer not happening. Can any one suggest how to send LIS2DW12 accelerometer sensor into sleep what are the register need to configure. if some one share sampl...

Resolved! LSM303AGR temperature compensation

Temperature compensation for this magnetometer is not working as I expect. When heating device from room temperature to 50-60 degrees Celsius in 3 minutes magnetometer values are changing a lot. I have 100Hz ODR, high-precision mode, temperature sens...

MHuk by Associate II
  • 2923 Views
  • 5 replies
  • 1 kudos

Resolved! How to handle e-Compass thermal drift

We do some initial validation of LIS3MDL and experienced a problem when we do a temperature cycle (20°C to 80°C in 20 minutes) in an oven with 7 sensors inside and no external magnetic field present.It seems that we get an offset in the output signal...

SensorTile.box USB connection does not work.

I am trying to work through the labs from the recent ST sensors workshop. The very first step in the Pro-mode lab is to enter the DFU mode and program the SensorTile.box with a precompiled image. The problem is that when I connect the tile to my co...

Rita Ch. by Associate II
  • 3094 Views
  • 4 replies
  • 0 kudos

LSM9DS1 BDU Details

Hi everyone,Does the block data update mode block also the sensor's sampling? Or simply the sensor continues to acquire and the registers are just not updated until the next reading? It's very important to me because I use LSM9DS1 gyroscope and accel...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.