MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems calibrating VL53L0X ToF distance sensor (VL53L0X_perform_offset_calibration, VL53L0X_perform_xtalk_calibration). bug?

RoutineVL53L0X_perform_offset_calibration from src/core/src/vl53l0x_api_calibration.cpp is giving strange results. By my opinion the problem is in uint16_t sum_ranging which should be of type uint32_t due to later bit shifting (<<16), which needs to ...

GPodr.1 by Associate II
  • 843 Views
  • 0 replies
  • 0 kudos

multiple VL53L0x interfacig with atmega 2560

I want to interface 3 VL53L0x with atmega 2560 using arv-gcc and not arduino but i am unable to do so I have its documet but i dont understand how to implement please .Please help me to interfcae all sensor and read all of them at same time

AJHA.11 by Associate
  • 685 Views
  • 0 replies
  • 0 kudos

Bandwidth vs ODR

Hi,I would like to know what is the difference between bandwidth and ODR. I tough that just the analog accelerometers have bandwidth and the digital ones have ODR. For example, IIS3DWB can go up to 5kHz bandwidth and 26.7kHz ODR. Does this means that...

LSM6DS3TR-C thermal charactersitics.

Please share the below details for LSM6DS3TR-C,1. Junction to ambient thermal resistance?2. Junction to case thermal resistance?3. Maximum operating case temperature?4 .Maximum operating junction temperature?

SR.1498 by Associate
  • 1144 Views
  • 1 replies
  • 0 kudos

LIS2DW12 hardware review

Find the attached schematic and review the same.Here we are using I2C communication.CS pin is directly connected to the MCU

MG.2362 by Associate II
  • 1850 Views
  • 2 replies
  • 0 kudos

Lsm6dsox interrupt on every sample?

Hi,I have a lsm6dsox sensor and everything is working fine, I can read the data and I can generate interrupts for single tap, double tap... But I want to configure as following:To set the sample rate at 52Hz, and every time it reads a sample to gener...

suads by Associate III
  • 1187 Views
  • 2 replies
  • 0 kudos

I am performing the self-test for the LIS2DW12 accelerometer. For some axes, when I compare data with and without the self-test enabled, I am getting a large difference in acceleration. Do I need to account for buffer overflow?

For example, given the following data taken from the sensor should the Y reading marked with a * account for a buffer overflow and therefore the difference be calculated as follows: 0xffff - 0xffd4 + 0x0e88 = 0x0eb3Initial X Reading:        0x0068Se...