MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SensorTile.box does not work sometimes

Hello, I'm trying to measure a few things unsing the SensorTile.box. Sometimes everything works fine but then the SensorTile.box seems to be dead all of a sudden. When I then try to connect it to my Windows pc, the pc won't recognise it and my phone ...

I'm using Shimmer 2r and I need to write on SD card using TinyOs and FatFS. I always get FR_DISK_ERROR when I try to open file; both if it exists and if it not. I tried to format SD: nothing change. How can I solve?

This is my TestSD_C.ns file:#define NEW_PRINTF_SEMANTICS#include "printf.h"#include "FatFs.h"configuration TestSD_C {}implementation { components MainC, TestSD_P; TestSD_P -> MainC.Boot; components FatFsP, diskIOC; TestSD_P.FatFs -> FatFsP; ...

FManc.1 by Associate II
  • 1173 Views
  • 1 replies
  • 0 kudos

[lsm303agr] How to get temperature sensor value correctly?

It is always 0 to get the value of OUT_TEMP_L_A (0Ch), OUT_TEMP_H_A (0Dh).Before reading OUT_TEMP_L_A (0Ch), OUT_TEMP_H_A (0Dh), check the values of TEMP_CFG_REG_A (1Fh), CTRL_REG4_A (23h) and STATUS_REG_AUX_A (07h) as bellow:TEMP_CFG_REG_A (1Fh): 0x...

Resolved! STMicro's Unicleo-GUI PC Application breaks when connecting through STMicro's ST-LINK in-circuit debugger and programmer pod. Why? [SOLVED]

Hi,I have used the STMicro's Unicleo-GUI PC Application to test both the LSM9DS1 STMicro's HAL and STMicro's Compass Middle Ware (from X-CUBE-MEMS1) - and - the LSM6DSO-LIS2MDL combination using almost the same software. All STMicro code (HAL for th...

Rstua.1 by Senior
  • 2918 Views
  • 8 replies
  • 0 kudos

LPS22HH not responding to pressure changes

I'm testing the LPS22HH on the MKI192-V1 eval board. At normal atmospheric pressure it reports about 1013 hPa, which is what I expect, and it fluctuates over time by a few hPa. It also reports a reasonable temperature value, so I know the I2C interfa...

TFras.1 by Associate
  • 938 Views
  • 0 replies
  • 0 kudos

Gyro & Accelerometer Linearity Specs for ISM330DHCX and LSM6DSM

I'm working on selecting between ISM330DHCX and LSM6DSM for some products under development. The one key sensor specification I can't find the data sheets is Typical Gyro/Accelerometer Nonlinearity (Best-fit straight Line) (% of FS). Can anyone poi...

SLibe by Associate II
  • 1916 Views
  • 3 replies
  • 0 kudos

How to perform a factory reset for SensorTile?

Hi Is there a way to perform a factory reset for SensorTile? For some reason, my laptop can't detect it anymore. Device manager said "This device cannot start. (Code 10). A device which does not exist was specified." I try to erase full chip flash me...

DWang by Associate II
  • 10218 Views
  • 31 replies
  • 0 kudos