MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS2DH datasheet : soldering information unclear

in the datasheet in section 3.1, it is mentioned to leave "pin 1 indicator" unconnected during soldering. Can this be clarified? Pin 1 is a functional pin and is always connected for a clock signal. How can we use this device if it is not allowed to...

LScho.1 by Associate
  • 874 Views
  • 1 replies
  • 0 kudos

LSM6DSOX : FSM interruption working only once after flashing. When I turn off and turn on again the device, the FSM does not work anymore ... Did I make a mistake in FSM configuration ?

Hello,I use the accelerometer LSM6DSOX. I want to get an interruption when the norm is above 8g. So I try to use the FSM and configure it. When I flash (for the first time) the system, everything works perfect ! But when I remove my battery and put i...

LIS3DH configuration setting for INT2

I have seen that this query has been asked previously but there was no answer to it.Therefore, I am raising the issue again here as follows: Currently, I am using INT1 for free fall detection which is already outlined in the AN3308 application note. ...

LIS2HH12 datasheet (rev 5) errata: purpose of DFC bits

Not sure if this belongs to the forum or whether I should better file a support request.I'm referring to revision 5 of the datasheet of LIS2HH12.On page 33, table 27, the function of the DFC bits are misrepresented as a high-pass cutoff frequency ins...

I need help to develoop my own firmware for STEVAL-MKSBOX1V1

I'm doing a final project with the STEVAL-MKSBOX1V1. I need to read temperature and sleep the tile box for a long period to save batery. I've never worked with MCUs, only with computers. Someone kwnows where I can find information about how to do it?...

NMart.1 by Associate III
  • 1766 Views
  • 4 replies
  • 0 kudos

IIS3DWB return zero

Hi,I'm trying to get an IIS3DWB up and running. If I read the register "WHO_AM_I", however, I only get "0" back! The SDO signal changes from "1" to "0" after 8 clk cycles and only changes again when CS becomes high.The IIS3DWB data sheet does not con...

FAsch by Associate II
  • 1078 Views
  • 1 replies
  • 0 kudos

IIS3DWB - Missing details in datasheet?

When configuring function routing on INT1/INT2 register (MD1_CFG/MD2_CFG), there is a note that says; "Activity/Inactivity interrupt mode (sleep change or sleep status) depends on the SLEEP_STATUS_ON_INT bit in SLOPE_EN (56h) register.But the SLOPE_E...

TResell by Associate II
  • 1178 Views
  • 1 replies
  • 0 kudos