User Activity

HelloIm using steval mksbox 1vs1 for vibration analysis. I have taken measurements with motor in movement and withe the motor stopped. At first I supose that with the motor in stop mode, the acc values in the 3 axis should be near to 0. In other thre...
I'm using STEVAL-MKSBOX1V1 for vibration analysis and I want to change sampling frecuency. I did it in the past with other versions of the project but now it has chan a little. I changed the ODR in the file lsm6dsox.c , but I also need to change the ...
HelloI know that tilebox has a RTC module, so I realise it is psoible to get current time for generating timestamp for data. Is it posible to do it? Is there any implementation of that in given project examples? Thank you
Hello, I'm using stm32 tilebox (STEVAL-MKSBOX1V1 )for vibration analysis. I need to change the smapling frecuency. Where is the parameter to change it? I'm using the BLEsensors application of FP-SNS-STBOX1.Thanks
HelloI had download the firmware FP-SNS-ALLMEMS2 on my STEVAL-MKSBOX1V1. From de app I can read the batery level, and I want to do the same with my raspberry and using bluepy. I have a script where I read the temperature and humidity values, so I wan...