MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am looking to make audio circuit

I am looking to make audio circuit. I need suggestion for microphone followed by noise cancellation ICs. Any help will be appreciated.ThanksSudhanshu.

SMeht.1 by Associate II
  • 4915 Views
  • 11 replies
  • 0 kudos

Resolved! How control Digital MEMS(MP45DT02)?

Hello, ​I am testing the MP45DT02 microphone on 32F4Discovery Board.​The final goal is to measure the sensitivity of the microphone(SPL) when you operate a buzzer with a frequency of 1 kHz.​First I set up the I2S communication as below to activate th...

0690X00000DXJx5QAH.png 0690X00000DXJlxQAH.png 0690X00000DXJm2QAH.png
DSEO by Associate II
  • 2889 Views
  • 2 replies
  • 0 kudos

Resolved! Sensor axis values are not consistent at higher ODR for LSM6DSO.

Hello,I am currently working with LSM6DSO and FIFO functionality.When ODR is set at 52Hz, axis values are correct but when I switch to 104Hz or 208Hz, values are not consistent. I have added my sensor configuration code and image to better explanatio...

0690X00000DAWITQA5.png
ASoni.2 by Associate III
  • 3717 Views
  • 4 replies
  • 0 kudos

LSM303AGR SPI Read Problem

HiI have lsm303agr mems sensor with stm32g4. It uses 3 wire SPI mode. I have problem with SPI communication. I used CubeMX with HAL mode and STMems_Standard_C_drivers for lsm303. The problem is that, when i read whoami register it reads 0x33 which is...

AAYKA.1 by Associate II
  • 2717 Views
  • 4 replies
  • 0 kudos

Not able to read accurate X, Y, Z, values of gyroscope

Hi Team,I am working with lsm6dsl 6 axis sensor , connected MT7621 processor via I2C.I would like to use gyro sensor only and followed the below setting in user space application.CTRL2_G (11h) = 0x60 (Gyro full scale 250dps, 416hz)INT1_CTRL (0Dh) = 0...

Vpava.1 by Associate
  • 1192 Views
  • 1 replies
  • 0 kudos

Why the LIS2DW12 is going into the power-down mode on restart?

(newbie)I'm configuring the registers using the STEVAL-MKI179V1 & STEVAL-MKI109V3 using Unico (see attached please)I'm planning to use int1=double_tap, int2=sleep/wakeup and to pull over spi from time to time the data (continuous mode).After i config...

0690X00000D8w86QAB.jpg
BPiti.1 by Associate
  • 1084 Views
  • 1 replies
  • 0 kudos