MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interface ISM330DLC with MEMS Adapter MKI109V3?

Hallo to All,we would like to put the ISM330DLC into a new product in developing, in order to evaluate in REAL TIME the overall vibrations in order to keep the operator in the SAFE OPERATING AREA.The tool is an electrical manual tool, an orbital sand...

FCern by Associate II
  • 1656 Views
  • 2 replies
  • 0 kudos

Why does the data-log code furnished with the sensor tile kit not work reliably? I am including all error codes and will copy the complete code if needed. Thanks, Ralph

Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48) Licensed under GNU GPL v2 For bug reports, read http://openocd.org/doc/doxygen/bugs.html srst_only separate srst_nogate srst_open_drain connect_assert_srst Info : The selected transp...

RTrim.1 by Associate
  • 1704 Views
  • 2 replies
  • 0 kudos

Infrasound response of MP34DT06J ?

Hi, do you have data and information about infrasound characteristics of MP34DT06J ? I looked at its frequency response in the data sheet, but information is being plotted starting from 100 Hz only. I'm using the CCA02M2 board.Many thanks!

MSant.11 by Associate III
  • 1558 Views
  • 3 replies
  • 0 kudos

SensorTile Datalog to SD cannot reach 500 Hz?

I am using STSW-STLKT01_V2.1.1 package Datalog project to program the sensortile. It works perfectly at 200Hz logging acc+ gyro+ Magnetometer data. I disabled all other sensors. However, if I increase the logging frequency to 500 Hz, it work for 5 se...

JWu.3 by Associate
  • 1122 Views
  • 1 replies
  • 0 kudos

Unknown USB Device (Device Descriptor Request Failed)

Hello,Trying to enter in DFU mode with the STM32CubeProg tool I get an unknown USB device error whenever I connect the SensorTile.box to my computer.The installation of the STM32CubeProg tool included the ST-LINK drivers and the usbser port driver pa...

GRobl by Associate II
  • 4545 Views
  • 2 replies
  • 0 kudos

Values from A3G4250D gyroscope have random ~1dps jumps

Hello, we're using A3G4250D in our project, and get data from it successfully in the stream mode, but, it accured, that from time to time there are random steps in the output data, and we have no clue on what can cause them. Did anyone meet such issu...

RZhar.1 by Associate
  • 1678 Views
  • 1 replies
  • 0 kudos

IIS2DH datasheet : soldering information unclear

in the datasheet in section 3.1, it is mentioned to leave "pin 1 indicator" unconnected during soldering. Can this be clarified? Pin 1 is a functional pin and is always connected for a clock signal. How can we use this device if it is not allowed to...

LScho.1 by Associate
  • 885 Views
  • 1 replies
  • 0 kudos

LSM6DSOX : FSM interruption working only once after flashing. When I turn off and turn on again the device, the FSM does not work anymore ... Did I make a mistake in FSM configuration ?

Hello,I use the accelerometer LSM6DSOX. I want to get an interruption when the norm is above 8g. So I try to use the FSM and configure it. When I flash (for the first time) the system, everything works perfect ! But when I remove my battery and put i...