MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

what are the units of the h3lis331dl output data?

Hi, I am using h3lis331dl to measure acceleration. I am using the official demo code, and I can get the ID correctly. But when I was trying to get acceleration data, the output data is weird. The output data in hexadecimal are:data_raw_acceleration....

YLiu.34 by Associate II
  • 1306 Views
  • 1 replies
  • 0 kudos

LSM6DSO issue connecting to AUX SPI

Hi,I have trouble using LSM6DSO via the AUX SPI - MISO is always high.I verified via the primary interface (I2C) that register WHO_AM_I (0Fh) returns 6Ch.I tried to change VDD after reading this post:VDD=3.3V: reading register CTRL1_OIS (70h) with th...

Yiftah by Associate II
  • 2991 Views
  • 8 replies
  • 0 kudos

Resolved! I can't read register WhoAmI from LIS2DW12 with I2C

Hi,I've bought a ST MKI179V1 board to interface via I2C with a Nucelo-L433RC . Furthermore, I'm using ST oficial drivers to MEMS sensors. The problem is when I try to read the register it always return 0. I've already made a lot of tests and I can't ...

0693W000000VxzoQAC.png
MAndr.233 by Associate III
  • 1760 Views
  • 3 replies
  • 0 kudos

STM32 STEVAL-MKSBOX1V1 is not working

Good day!I recently uploaded a .bin file in the stm32 using STM32 Prog, after downloading, the LED of the stm32 doesn't blink anymore and there is no response in the computer when I tried to plug it in using usb port and also there is no device found...

ICabi.1 by Associate
  • 1204 Views
  • 1 replies
  • 0 kudos