cancel
Showing results for 
Search instead for 
Did you mean: 

Please share the below details for LSM6DS3TR-C, 1. Junction to ambient thermal resistance? 2. Junction to case thermal resistance? 3. Maximum operating case temperature? 4 .Maximum operating junction temperature?

SR.1498
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @SR.1498​ , for which application do you need these details? Pls consider that the LSM6DS3TR max supply is 3.6V and max current (high performance mode, max ODR) is 1250uA, so the power consumed in the worst case is P=V*I=4,5mW. If you consider that the device package thermal resistance is typ 80°C/W, the thermal difference between the device and the environment is DeltaT=0.3°C worst case. The maximum operating junction is basically the abs max rating in the datasheet. Regards