MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Mems studio fsm debug

I am using Mems-Studio for my FSM project. I am testing the state machine, and everything is working fine; I can see interrupts. However, in the debug tab, when debug mode is enabled, the table does not compile, and I cannot observe the program's beh...

SamuPre_0-1738754405575.png
SamuPre by Associate
  • 1100 Views
  • 1 replies
  • 0 kudos

LPS22HBTR pressure range query

Dear ST/Forum,Preamble:We are using the LPS22HBTR pressure-temperature sensor in some PCB assemblies.The data sheet indicates a pressure reading range with defined accuracy from 260 to 1260hPA/millibar and an absolute maximum overpressure value of 2M...

DuncanR by Associate II
  • 425 Views
  • 0 replies
  • 0 kudos

ILPS22QS: SWRESET bit not clearing

We are currently trying to run experiments with the ILPS22QS sensor. According to the datasheet, when setting the SWRESET bit in the CTRL2 register to 1, it should self-clear when the reset is finished - but this never happens. The bit stays 1, and t...

ISM330DLC misalignment measurement result

Hi, I use the ISM330DLC to measure the tilting of an excavator arm (similar to an inclinometer). I have observed that some ISM330DLC accelerometer sensors exhibit misalignment in their Z-axis measurements. For example, while the X and Y axes produce ...

deddy11 by Associate II
  • 461 Views
  • 3 replies
  • 0 kudos

LSM6DSL Power Consumption

Hello,I am writing a firmware with nrf52832 microcontroller and I have interfaced ST's LSM6DSL module. I am facing some issues regarding power consumption of LSM6DSL module. I have used 10K resistors with sda, scl, sdO and cs pins is this correct.I a...

yash2530 by Associate II
  • 2234 Views
  • 5 replies
  • 1 kudos

Resolved! ISM330DLC fifo settings issue

HiI managed to read both accelerometer and gyroscope ISM330DLC in "polling" mode with INT1 pin with 3330 output data rate, but my goal is to reach peak data rate (6660 samples / s) so I need to use FIFO and this is where my problems start, I dont kno...

amistar by Associate III
  • 1035 Views
  • 7 replies
  • 0 kudos

Resolved! LIS2MDL BDU only works for 3 axis independent readouts

HI, it seems to me that reading the LIS2MDL sensor only works correctly if I read first the X axis, then the Y axis, and finally the Z axis separately, each axis in a separate SPI transaction. My settings:- continuous measurement, output data rate se...

amistar by Associate III
  • 893 Views
  • 4 replies
  • 0 kudos