MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sensor Recommendation for Vibration and Motion Detection

Hi, We are developing a product/device that is mounted on a machine/vehicle that generates vibrations when in the ON state. We need a sensor that can 1.. Detect vibration start and stop while the device is stationary, with good accuracy, to determine...

Jayk by Associate
  • 700 Views
  • 6 replies
  • 0 kudos

Resolved! FSM double tap

Hi, I'm trying to implement the tap and double-tap function in the FSM tab. Is it possible to achieve this at an output data rate of 26 Hz? 

SamuPre by Associate
  • 1162 Views
  • 1 replies
  • 1 kudos

Continuously varying output from MEMS Gyroscope

We are using the X-STM32MP-GNSS2 (with the STM32 discovery board DK2), which has ISM330DHCX IMU. The accelerometer readings seem fine from the IMU, but the gyroscope gives enormously high and varying readings even when we are stationary. See below th...

STEVAL-PROTEUS: Serial Monitor over Micro USB

Hi all!I've recently started working on a fault classification model utilizing the proteus1 board and the NEAI studio suite. I'd ideally like to set up a serial datalogger via the onboard micro USB to both obtain and display readings, alongside bench...

Haze by Associate II
  • 1130 Views
  • 2 replies
  • 0 kudos

Resolved! ST notifies termination of the following product: LIS3MDLTR

We embed LIS3MDLTR on our board that we produce, because this has high sensitivity: 6842 LSB/gauss. This corresponds to 0.146 mgauss/LSB, if I convert correctly. The other products has significanltly lower sensitivity: 1.5 mgauss/LSB. What are you pr...

tcseh by Associate
  • 2333 Views
  • 11 replies
  • 5 kudos

LPS22HBTR and PCB cleaning

Dear ST/Forum,We are using the LPS22HBTR pressure-temperature sensor in some PCB assemblies.Due to some cleanliness requirements of the experiment, I need to be able to clean the PCB this device is attached to but due to the very fine holes in the li...

DuncanR by Associate II
  • 1598 Views
  • 4 replies
  • 0 kudos

Resolved! ST1VAFE3BX basic MEMS Studio not behaving as expected

Are there any plans to have a video tutorial on the biosensor eval board?  (ST1VAFE3BX)? I connected it to MEMS Studio via the MKI109V3.  I'm experimenting with the "Features Demo" but it's not behaving as I expect.  Perhaps there's documentation abo...

Rauscher by Associate II
  • 834 Views
  • 5 replies
  • 2 kudos