MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Programming an M24C02 with ST-Link/V2

I have bunch of M24C02 eeproms in some old equipment that I would like to reprogram. I have an ST-Link/V2 installed on an laptop running Windows 10. It has the STM32 STLink driver installed. I also have installed ST Visual Develop. Using this set of...

0693W000001cbd5QAA.png
TBodi.1 by Associate
  • 3514 Views
  • 4 replies
  • 0 kudos

Calibrating digital magnetometer along only two axis.

I am making a tilt-compensated digital compass with an MMC5983MA magnetometer and a LIS2HH12 accelerometer. I have been calibrating the compass using the min/max method and rotating the compass in free space, which works fairly well.I need to be able...

CGrov.1 by Associate II
  • 1574 Views
  • 2 replies
  • 0 kudos

What if I use a power supply of 3.3v for the LSM9DS1 module?

Hi, in the module specifications (bottom of page 12 of the datasheet) says:"The product is factory calibrated at 2.2 V. The operational power supply range is from 1.9 V to 3.6 V."But what happens if I use 3.3v instead 2.2v?, in the datasheet does not...

How to fix STEVAL-BFA001V1B PdM module on motor?

Hi,I am working with STEVAL-BFA001V1B module and want to fix this on a motor which is shown below. As there is no screw hole on this module so please suggest some method to attach this ?

0693W000001pIKUQA2.jpg
RJain.1 by Associate III
  • 520 Views
  • 1 replies
  • 0 kudos

Analog gyroscope solution

Hi everyone,I'm wondering if there is a solution from ST for a analog gyroscope eventually on 3-axis for a crash-test micro device for test and measuring that I'm designing.Basically I've found an old product from ST named LYPR540AH but it is obsolet...

AGall.1 by Associate II
  • 2979 Views
  • 10 replies
  • 0 kudos

Resolved! nucleo-gui can connecet uart port,but can not statrt

nucleo-gui can connecet uart port,but can not start, like follows​1.nucleo borad: nucleo-l4r5zi , mems borad: iks01a22. using X-CUBE-MEMS1 7.10 gesturerecognition appliction3.anyone know what is problem? thank you?​

0693W000001cZ8eQAE.png 0693W000001cZ9DQAU.png
Fgg by Associate II
  • 1362 Views
  • 5 replies
  • 0 kudos

LIS3DH Low Power Mode not working as expected.

Hello Everybody,I'm using LIS3DH Sensor to detect anomalous accelerations on a battery powered device.Is important, due to battery duration problems, to keep the current consumption as low as possible...I set the regisers as follows: write_I2C_LIS3DH...

The best approach to write MEMS microphone values into an SD CARD

Hello everyone,I have been programming a MEMS microphone with a desirable rate of 48KHz. I'm working on a STM32L433 Nucleo Board and the data from microphone is being acquired via DMA with SAI protocol. I process the PDM data to PCM through PDM2PCM l...

ALope.1 by Associate II
  • 963 Views
  • 1 replies
  • 0 kudos