Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi,I'm facing with a issue on unicleo gui and sensorTile sensor (with ALLMEMS1 and ALLMEMS2 librairies).I dont know why, but since few day i can pair and connect my sensor tile with bluetooth on my laptop (W10) but unicleo doesn't show the normal in...
When I am changing the number of channels to 1 channel.it is recognized by the windows driver, but the"advanced" TAB is disappear (unlike 2 channels configuration). Did someone faced with this kind problem? Do I missedsomething? of course, audacity d...
Which firmware version should be on sensortile box? Any other recommendations is much appreciated.I am having issues with 2 of 2 sensortile boxes I received yesterday. All interactions have been with Android st ble app. No response from one and...
Hello,I need to use dual MEMS (ISM330DHCX) and MCU in my application for redundancy. Each MEMS is connected to a different MCU with independent supply. The data collected from sensors will be crossed checked if within a predefined tolerance. I think ...
Please I really need help, I am using the P-Nucleo VL6180X, the purpose of my job is to command the opening of a door normally but before that I would already like to succeed in ordering the lighting of an LED.I use the stmicro API which I am trying ...
We have a small percentage of devices that once powered on show a certain issue.One or more axes of the accelerometer values are capped to the max or minimum value.This issue disappears when the device is powered off and powered back on.All the regis...
HI All, I am using STWIN-STWINK1 for a predictive maintenance application, I am unable to set up SWV ITM data console and trace on STM32CubeIDE. I tried following all the tutorials on YouTube and community, nothing works. If anyone has been able to g...
arm-none-eabi-u_printf_float -o "STWIN_WiFi_Connectivity.elf" @"objects.list" -mcpu=cortex-m4 -T"E:\SANAVA_PROJECTS\Vibration Sensor\cloud_wifi\STSW-STWINKT01_V2.0.0\Projects\WiFi_Connectivity\STM32CubeIDE\STWIN_WiFi_Connectivity\STM32L4R9ZITx_FLASH...
Dear sir,We are using your company's three-dimensional acceleration chip LIS2DS12. Now we have found a fatal defect. When the ambient temperature value detected by the temperature sensor inside the chip changes from 24 ℃ to 25℃, the acceleration out...