cancel
Showing results for 
Search instead for 
Did you mean: 

HTS221 Temperature measuring

AFeil.1445
Associate

Hi,

we are using HTS221TR. In the datasheet it is not clear what is the temperature range what the sensor can measure -40...85? +15°C....40?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @AFeil.1445​ , the HTS221 can detect the temperature in the entire -40°C...+120°C range, but with different accuracies centered around 25°C, which is the calibration point:

  • typ +-0.5 between 15°C and 40°C
  • typ +-1 from 0°C to 15°C and from 40°C to 60°C
  • typ +-2 from -40°C to 0°C and from 60°C to 120°C

(p.8 of the datasheet)

0693W000001pupRQAQ.png

Regards