Skip to main content
TMCGE.1
Associate
May 14, 2020
Question

100-3000 psi pressure sensor to long distance WIFI.

  • May 14, 2020
  • 2 replies
  • 973 views

I want to build a communications device that looks at 100-3000 psi pressures in my chemical plant and transmits the data to a receiver and GUI in the control room on a dedicated workstation. I am thinking it will take a .5-4.5 VDC pressure transducer, a ADC that will allow multiple pressure transducers to input and output. A controller that can manage the data transmits, and a WIFI transmitter.

On the receiving end, I am looking at a WIFI receiver and a controller that can convert the data and input it into a GUI.

I need help identifying what the exact parts I need are.

Can anyone help?

This topic has been closed for replies.

2 replies

Eleon BORLINI
ST Employee
May 15, 2020

Hi @TMCGE.1​ , I could suggest you to check the STWIN kit and especially its Wifi module, the STEVAL-STWINWFV1. The onboard module can be used together with the STWIN software, or it can be considered as stand alone: in this second could be a starting point to check the device specs and resources page. Btw, which cpecific kind of pressure sensor are you trying to configure? Regards

TMCGE.1
TMCGE.1Author
Associate
May 15, 2020

Thanks for the lead! I was looking into the following sensor for the cos and specs. Honeywell MLH08KPSB01A Industrial Pressure Sensor 8000 PSI .5-4.5 VDC OUT T122119

Piranha
Principal III
May 30, 2020

Don't call "anything wireless" a Wi-Fi, because Wi-Fi is a name of specific technology - IEEE 802.11 wireless networking. In your case it sounds like you need LoRa:

https://www.st.com/content/ccc/resource/sales_and_marketing/presentation/product_presentation/group0/b5/72/c6/ec/c8/e3/4a/8c/IoTaugmented_stm32-lrwan/files/IoTaugmented_stm32-lrwan.pdf/jcr:content/translations/en.IoTaugmented_stm32-lrwan.pdf