2020-06-01 1:32 AM
According to the official sample program, I set the register to detect free-fall event,But it can't be detected very well, even when I haven't moved anything, I have always detected the free-fall event,How can I use lsm6dso to detect free-fall event correctly?
2020-06-01 1:34 AM
2020-06-01 1:54 AM
Hi @Ljian.1 , on which part number did you managed to detect the free-fall event, before LSM6DSO? You could try to change the detection threshold to a lower value and check if you can detect the free-fall interrupt.
/* Set Free Fall duration to 3 and 6 samples event duration */
lsm6dso_ff_dur_set(&dev_ctx, 0x06);
lsm6dso_ff_threshold_set(&dev_ctx, LSM6DSO_FF_TSH_312mg);Regards
2020-06-01 2:04 AM
This is the first time I have used lsm6dso to detect free-fall events. I have not used other ones before.
I changed the detection threshold to a lower value still not work!
2020-06-01 2:06 AM
This is my enable free-fall detection sourcecode.
void static FallDetectionInit(void)
{
//stmdev_ctx_t dev_ctx;
lsm6dso_pin_int1_route_t int1_route;
/*
* Uncomment to configure INT 2
*/
//lsm6dso_pin_int2_route_t int2_route;
/*
* Initialize mems driver interface
*/
//dev_ctx.write_reg = platform_write;
//dev_ctx.read_reg = platform_read;
/*--------Enable free-fall detection from sensor(lsm6dso)--------*/
/* Enable LIR */
lsm6dso_int_notification_set(&dev_ctx, LSM6DSO_ALL_INT_LATCHED);
/* Set Free Fall duration to 3 and 6 samples event duration */
lsm6dso_ff_dur_set(&dev_ctx, 0x03);
lsm6dso_ff_threshold_set(&dev_ctx, LSM6DSO_FF_TSH_312mg);
/*--------Enable detect activity/inactivity from sensor(lsm6dso)--------*/
/* Set duration for Activity detection to 9.6 ms (= 4 * 1 / ODR_XL) */
lsm6dso_wkup_dur_set(&dev_ctx, 0x04);
/* Set duration for Inactivity detection to 4.92 s (= 4 * 512 / ODR_XL) */
lsm6dso_act_sleep_dur_set(&dev_ctx, 0x04);
/* Set Activity/Inactivity threshold to 62.5 mg */
lsm6dso_wkup_threshold_set(&dev_ctx, 0x02);
/*
* Inactivity configuration: XL to 12.5 in LP, gyro to Power-Down
*/
lsm6dso_act_mode_set(&dev_ctx, LSM6DSO_XL_12Hz5_GY_PD);
/*
* Enable interrupt generation on Inactivity INT1 pin
*/
lsm6dso_pin_int1_route_get(&dev_ctx, &int1_route);
int1_route.md1_cfg.int1_ff = PROPERTY_ENABLE;
lsm6dso_pin_int1_route_set(&dev_ctx, &int1_route);
/* initialize variables */
fall_occur = FALL_DETECT_FALSE;
fall_detect_status = FALL_DETECT_STATUS_NONE;
return;
}