MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM303DLHC software

Hi ThereWhere I can find some source files for LSM303DLHCI see some ref.links there, but right now they pointed to non-existed pages on github :( Or I miss somethingAlso I found this link https://github.com/STMicroelectronics/stm32-lsm303dlhc but it ...

LPS22HBTR sensor data error.

Dear ST/Forum,Your attention would be much appreciated for a technical enquiry.We are using the LPS22HB pressure and temperature sensors in some electronics for an experiment that will be onboard the International Space Station (ISS) in orbit later t...

DuncanR by Associate II
  • 220 Views
  • 2 replies
  • 0 kudos

Sensor Recommendation for Vibration and Motion Detection

Hi, We are developing a product/device that is mounted on a machine/vehicle that generates vibrations when in the ON state. We need a sensor that can 1.. Detect vibration start and stop while the device is stationary, with good accuracy, to determine...

Jayk by Associate
  • 145 Views
  • 6 replies
  • 0 kudos

Resolved! FSM double tap

Hi, I'm trying to implement the tap and double-tap function in the FSM tab. Is it possible to achieve this at an output data rate of 26 Hz? 

SamuPre by Associate
  • 156 Views
  • 1 replies
  • 1 kudos

ISM330DLC FIFO AXL+Gyro+Timestamp

Dear SupportI want to add timestamp registration to the FIFO.I already use FIFO to save gyroscope and accelerometer samples, but I'm struggling to add timestamps.Since ODR is too high for polling mode the only solution is this one.I attach some code ...

Screenshot 2025-02-05 155202.png

STHS34PF80 stuck in presence state

Hi All,I use STHS34PF80 for presence detection with embedded algorithm however it easily get stuck in presence status and cannot release from the status.Use case:People sit in from of the sensor around 30 cm, with lens on STHs34PF80.When people enter...

ibs09ps-annotate.png
SLin.11 by Associate III
  • 197 Views
  • 7 replies
  • 1 kudos

Continuously varying output from MEMS Gyroscope

We are using the X-STM32MP-GNSS2 (with the STM32 discovery board DK2), which has ISM330DHCX IMU. The accelerometer readings seem fine from the IMU, but the gyroscope gives enormously high and varying readings even when we are stationary. See below th...