2025-02-05 7:11 AM - edited 2025-02-05 7:19 AM
Dear Support
I want to add timestamp registration to the FIFO.
I already use FIFO to save gyroscope and accelerometer samples, but I'm struggling to add timestamps.
Since ODR is too high for polling mode the only solution is this one.
I attach some code snippets to make it clear, also consider them as pseudo code taken from a more complex structure.
ism330dlc_fifo_time_set and timer_rd are not present in the library but I wrote them based on the AN5125
int32_t ism330dlc_fifo_time_set(stmdev_ctx_t *ctx, uint8_t val) {
ism330dlc_fifo_ctrl2_t fifo_ctrl2;
int32_t ret;
ret = ism330dlc_read_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2,
1);
if (ret == 0) {
fifo_ctrl2.fifo_timer_en = val;
ret = ism330dlc_write_reg(ctx, ISM330DLC_FIFO_CTRL2,
(uint8_t *)&fifo_ctrl2, 1);
}
return ret;
}
uint64_t ism330dlc_timer_rd(stmdev_ctx_t *ctx) {
uint64_t time = 0;
uint8_t t0;
ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP0_REG, (uint8_t *)&t0, 1);
time = t0;
ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP1_REG, (uint8_t *)&t0, 1);
time |= uint64_t(t0 << 8);
ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP2_REG, (uint8_t *)&t0, 1);
time |= uint64_t(t0 << 16);
return time * 25;
}
void start_routine() {
sens.freq = 104u;
pattern_len = 18;
ism330dlc_block_data_update_set(&ctx.Ctx, PROPERTY_ENABLE);
ism330dlc_int1_route_t int_1_reg{};
ism330dlc_pin_int1_route_get(&ctx.Ctx, &int_1_reg);
int_1_reg.int1_fth = PROPERTY_ENABLE;
ism330dlc_pin_int1_route_set(&ctx.Ctx, int_1_reg);
ism330dlc_fifo_watermark_set(&ctx.Ctx, sens.freq * pattern_len);
ISM330DLC_ACC_Enable(&ctx);
ISM330DLC_GYRO_Enable(&ctx);
ISM330DLC_ACC_SetOutputDataRate(&ctx, sens.freq);
ISM330DLC_GYRO_SetOutputDataRate(&ctx, sens.freq);
ism330dlc_fifo_dataset_4_batch_set(&ctx.Ctx, ISM330DLC_FIFO_DS4_NO_DEC);
ism330dlc_fifo_xl_batch_set(&ctx.Ctx, ISM330DLC_FIFO_XL_NO_DEC);
ism330dlc_fifo_gy_batch_set(&ctx.Ctx, ISM330DLC_FIFO_GY_NO_DEC);
ism330dlc_timestamp_res_set(&ctx.Ctx, ISM330DLC_LSB_25us);
// ism330dlc_timer_int_set(&ctx.Ctx, 1);
ism330dlc_timestamp_set(&ctx.Ctx, 1);
ism330dlc_fifo_time_set(&ctx.Ctx, 1);
ISM330DLC_FIFO_Set_ODR_Value(&ctx, sens.freq);
ism330dlc_fifo_mode_set(&ctx.Ctx, ISM330DLC_STREAM_MODE);
}
void loop(){
int16_t num;
ism330dlc_fifo_data_level_get(&ctx.Ctx, &num);
for (auto i = 0u; i < num; i++) {
uint16_t pat;
axis ax[3]{};
ism330dlc_fifo_pattern_get(&ctx.Ctx, &pat);
auto &v = ax[pat / 3].ax.i16bit[pat % 3];
ism330dlc_fifo_raw_data_get(&ctx.Ctx, (uint8_t *)&v, sizeof(v));
auto m = (pat < 3) ? sens.gy / 1000
: pat < 6 ? sens.axl / 1000
: 25;
auto e = su::stringify(float(v) * m, 2);
auto tm = ism330dlc_timer_rd(&ctx.Ctx);
slog::println("IMU", [&]() {
return su::stringify(tm) + " pat " + su::stringify(pat) + " " +
e;
}());
}
}
Notes:
- trying different ODRs makes the same results
- enabling/disabling BDU won't change anything
- Loop() is called in a task when the IRQ is triggered
results: Timestamp in polling + #pattern + converted gy/axl and zero timestamp
Looking forward to hearing from you,
Best regards,
Andrea
Solved! Go to Solution.
2025-02-27 9:10 AM - edited 2025-02-27 9:11 AM
I opened this pull request
https://github.com/STMicroelectronics/stm32-ism330dlc/pull/2
The problem was there so this fixed the issue
2025-02-06 1:23 AM
Hi @andross092 ,
To add timestamp registration to your FIFO data, you can follow these steps:
Try these functions with for the timestamp functionality:
%Function to Set FIFO Time
int32_t ism330dlc_fifo_time_set(stmdev_ctx_t *ctx, uint8_t val) {
ism330dlc_fifo_ctrl2_t fifo_ctrl2;
int32_t ret;
ret = ism330dlc_read_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2, 1);
if (ret == 0) {
fifo_ctrl2.fifo_timer_en = val;
ret = ism330dlc_write_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2, 1);
}
return ret;
}%Function to Read Timer
uint64_t ism330dlc_timer_rd(stmdev_ctx_t *ctx) {
uint64_t time = 0;
uint8_t t0;
ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP0_REG, (uint8_t *)&t0, 1);
time = t0;
ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP1_REG, (uint8_t *)&t0, 1);
time |= uint64_t(t0 << 8);
ism330dlc_read_reg(ctx, ISM330DLC_TIMESTAMP2_REG, (uint8_t *)&t0, 1);
time |= uint64_t(t0 << 16);
return time * 25; // Assuming 25us resolution
}
2025-02-06 3:33 AM
Hi Federica
Thanks for your reply.
Since those were my functions and you just copied them I suppose what I'm trying to do is already correct.
But as you can see from my logs those configurations aren't working as expected, because I cannot retrieve any valid timestamp from the FIFO
2025-02-11 9:13 AM
Dear support,
Is there any update on the topic?
2025-02-26 2:14 PM
Did you set the batch data for batch #4 dedicated to timestamps?
ism330dlc_fifo_dataset_4_batch_set()
Then looking at the AN5125 it seems that bit #7 (128) must be set in FIFO_CTRL2 to enable the timestamps in batch #4 (you seem to set bit #0)
The corresponding function does not exist in the official driver on GitHub, but one can copy rename and change the similar function ism330dlc_fifo_temp_batch_set() that enables temperature in batch #4
let us know if this solves
2025-02-27 6:37 AM
HI Andrea,
Thanks for your reply.
I actually set that bit to one in this function
int32_t ism330dlc_fifo_time_set(stmdev_ctx_t *ctx, uint8_t val) {
ism330dlc_fifo_ctrl2_t fifo_ctrl2;
int32_t ret;
ret = ism330dlc_read_reg(ctx, ISM330DLC_FIFO_CTRL2, (uint8_t *)&fifo_ctrl2,
1);
if (ret == 0) {
fifo_ctrl2.fifo_timer_en = val;
ret = ism330dlc_write_reg(ctx, ISM330DLC_FIFO_CTRL2,
(uint8_t *)&fifo_ctrl2, 1);
}
return ret;
}when I call
ism330dlc_fifo_time_set(&ctx.Ctx, 1);in the init
but since you highlighted the fact that is the 7th bit I guess I have an answer:
Take a look at ism330dlc_reg.h:
this struct splits register in 9bit instead of 8, so I don't know where I'm actually writing
2025-02-27 8:54 AM
agreed - in the official driver there is a bug: not_used_01:3 is the correct code for the bitfield definition of FIFO_CTRL2
will amend ASAP - let us know if this fixes your issue
also, can you reconfirm you set the batch #4 rate by writing to FIFO_CTRL4?
2025-02-27 9:10 AM - edited 2025-02-27 9:11 AM
I opened this pull request
https://github.com/STMicroelectronics/stm32-ism330dlc/pull/2
The problem was there so this fixed the issue
2025-02-27 9:34 AM
glad we found the issue!